<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Difference between LPC Open and Library from lpcware git in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Difference-between-LPC-Open-and-Library-from-lpcware-git/m-p/576396#M19435</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by amoehl on Mon Apr 15 02:55:26 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;i am a little confused. Meanwhile i have two different libraries. One comes with Code Red Suite in the Example and is also here in the git:&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fgit.lpcware.com%2F%2Flpc43xx" rel="nofollow" target="_blank"&gt;http://git.lpcware.com//lpc43xx&lt;/A&gt;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;The other is the lpcOpen.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;It seems, that booth are made from NXP, but the name scheme and the folder structure are complete different. Currently i use the Lib from the git above.&lt;BR /&gt;But when i tried to use the USB Example, it doesn't work. So i tried to use the USB lib from lpcopen but this needs the&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;So, what should i use?? What are the Pro's and the Con's for the libraries?&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Andre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:01:52 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:01:52Z</dc:date>
    <item>
      <title>Difference between LPC Open and Library from lpcware git</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Difference-between-LPC-Open-and-Library-from-lpcware-git/m-p/576396#M19435</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by amoehl on Mon Apr 15 02:55:26 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;i am a little confused. Meanwhile i have two different libraries. One comes with Code Red Suite in the Example and is also here in the git:&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fgit.lpcware.com%2F%2Flpc43xx" rel="nofollow" target="_blank"&gt;http://git.lpcware.com//lpc43xx&lt;/A&gt;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;The other is the lpcOpen.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;It seems, that booth are made from NXP, but the name scheme and the folder structure are complete different. Currently i use the Lib from the git above.&lt;BR /&gt;But when i tried to use the USB Example, it doesn't work. So i tried to use the USB lib from lpcopen but this needs the&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;So, what should i use?? What are the Pro's and the Con's for the libraries?&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Andre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:01:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Difference-between-LPC-Open-and-Library-from-lpcware-git/m-p/576396#M19435</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:01:52Z</dc:date>
    </item>
  </channel>
</rss>