<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPCOpen 2.16 LPC43xx suggestions</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-2-16-LPC43xx-suggestions/m-p/576075#M19363</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by robekras on Thu Apr 09 07:20:00 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Some suggestions for changes to LPCOpen for LPC43xx&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1) Please remove the iap.h. There is a iap_18xx_43xx.h which is the right one.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2) Please introduce 'uint8_t Chip_IAP_Init (void);' to the iap_18xx_43xx.c/h. This is a necessary function to be called for erasing and writing the flash. It is mentioned in the manual UM10503.pdf, but it's missing in LPCOpen.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In UM10503.pdf it is stated, that the Init is giving back a CMD_SUCCESS (which is 0), but I don't observe any given back value. It is also not clear whether this function has to be called once, or every time before writing or erasing functions are called.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3) Please change the declaration and definition of iap_entry. In declaration and definition 'unsigned int' is used. But in the calling functions (in iap_18xx_43xx.c the arrays are of type uint32_t. This gives warning messages.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; Robert&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 20:15:35 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T20:15:35Z</dc:date>
    <item>
      <title>LPCOpen 2.16 LPC43xx suggestions</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-2-16-LPC43xx-suggestions/m-p/576075#M19363</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by robekras on Thu Apr 09 07:20:00 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Some suggestions for changes to LPCOpen for LPC43xx&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1) Please remove the iap.h. There is a iap_18xx_43xx.h which is the right one.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2) Please introduce 'uint8_t Chip_IAP_Init (void);' to the iap_18xx_43xx.c/h. This is a necessary function to be called for erasing and writing the flash. It is mentioned in the manual UM10503.pdf, but it's missing in LPCOpen.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In UM10503.pdf it is stated, that the Init is giving back a CMD_SUCCESS (which is 0), but I don't observe any given back value. It is also not clear whether this function has to be called once, or every time before writing or erasing functions are called.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3) Please change the declaration and definition of iap_entry. In declaration and definition 'unsigned int' is used. But in the calling functions (in iap_18xx_43xx.c the arrays are of type uint32_t. This gives warning messages.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; Robert&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:15:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-2-16-LPC43xx-suggestions/m-p/576075#M19363</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:15:35Z</dc:date>
    </item>
  </channel>
</rss>