<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC4357 power consumption issuse</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-power-consumption-issuse/m-p/576037#M19362</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by henna on Fri Jun 19 08:42:46 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am working on a project requires very low power consumption when not in active state.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;With reference to the LPC4357 manual both m4 and m0 core can be put into deep power down mode independently. To test this I put m0 core into deep power mode and m4 in active mode. In this case power consumption was 21mA and which was not significantly reduced.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In second test I put m4 in deep power down mode and m0 in sleep state, in this case power consumption was reduced to 6 mA.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am not sure is this is the lowest power I can go with dual or Is there is anyway to lower the power consumption below 6mA.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I can try putting both the core into deep power down which is one option, but can anybody suggest me some idea which I can implement to lower LPC4357 dual core MCU power consumption in deep power down mode or deep sleep mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any help will be appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Heena&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:04:10 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:04:10Z</dc:date>
    <item>
      <title>LPC4357 power consumption issuse</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-power-consumption-issuse/m-p/576037#M19362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by henna on Fri Jun 19 08:42:46 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am working on a project requires very low power consumption when not in active state.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;With reference to the LPC4357 manual both m4 and m0 core can be put into deep power down mode independently. To test this I put m0 core into deep power mode and m4 in active mode. In this case power consumption was 21mA and which was not significantly reduced.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In second test I put m4 in deep power down mode and m0 in sleep state, in this case power consumption was reduced to 6 mA.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am not sure is this is the lowest power I can go with dual or Is there is anyway to lower the power consumption below 6mA.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I can try putting both the core into deep power down which is one option, but can anybody suggest me some idea which I can implement to lower LPC4357 dual core MCU power consumption in deep power down mode or deep sleep mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any help will be appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Heena&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:04:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-power-consumption-issuse/m-p/576037#M19362</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:04:10Z</dc:date>
    </item>
  </channel>
</rss>