<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Which emWin should I use for LPC4088 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Which-emWin-should-I-use-for-LPC4088/m-p/575813#M19315</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The latest emWin V5.30c supports LPC4088 product.&lt;/P&gt;&lt;P&gt;I would recommend customer to download emWIN software for NXP product from &lt;A href="http://www.nxp.com/pages/emwin-graphics-library:EMWIN-GRAPHICS-LIBRARY"&gt;NXP emWin website&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Aug 2016 07:48:33 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2016-08-09T07:48:33Z</dc:date>
    <item>
      <title>Which emWin should I use for LPC4088</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Which-emWin-should-I-use-for-LPC4088/m-p/575812#M19314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the LPC4088 processor with 7" touch LCD. We plan to use emWin to develop a GUI interface for a project. I am currently working with version 5.22, but I see newer ones available on the NXP site. Should I download the latest?&lt;/P&gt;&lt;P&gt;It appears that 5.30c is available, is it compatible with LPC4088?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, do I have to download these libraries from NXP or can I go to the Segger site directly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Aug 2016 14:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Which-emWin-should-I-use-for-LPC4088/m-p/575812#M19314</guid>
      <dc:creator>mikemillsap</dc:creator>
      <dc:date>2016-08-05T14:59:43Z</dc:date>
    </item>
    <item>
      <title>Re: Which emWin should I use for LPC4088</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Which-emWin-should-I-use-for-LPC4088/m-p/575813#M19315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The latest emWin V5.30c supports LPC4088 product.&lt;/P&gt;&lt;P&gt;I would recommend customer to download emWIN software for NXP product from &lt;A href="http://www.nxp.com/pages/emwin-graphics-library:EMWIN-GRAPHICS-LIBRARY"&gt;NXP emWin website&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Aug 2016 07:48:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Which-emWin-should-I-use-for-LPC4088/m-p/575813#M19315</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-08-09T07:48:33Z</dc:date>
    </item>
  </channel>
</rss>