<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Chip_Clock_SetSysClockDiv in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Chip-Clock-SetSysClockDiv/m-p/575215#M19190</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by oxijin on Tue Jul 21 14:37:13 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the IRC oscillator on an LPC11xx.&amp;nbsp; The board has no crystal.&amp;nbsp; The micro will start up using the IRC oscillator.&amp;nbsp; Can I change the clock divider on the fly in board_sysinit.c, while running on the IRC oscillator, as follows?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;STATIC void SystemSetupClocking(void)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_Clock_SetSysClockDiv(2); &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It seems very likely that the answer is yes, but I just want to be sure.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 20:16:32 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T20:16:32Z</dc:date>
    <item>
      <title>Chip_Clock_SetSysClockDiv</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Chip-Clock-SetSysClockDiv/m-p/575215#M19190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by oxijin on Tue Jul 21 14:37:13 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the IRC oscillator on an LPC11xx.&amp;nbsp; The board has no crystal.&amp;nbsp; The micro will start up using the IRC oscillator.&amp;nbsp; Can I change the clock divider on the fly in board_sysinit.c, while running on the IRC oscillator, as follows?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;STATIC void SystemSetupClocking(void)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_Clock_SetSysClockDiv(2); &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It seems very likely that the answer is yes, but I just want to be sure.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:16:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Chip-Clock-SetSysClockDiv/m-p/575215#M19190</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:16:32Z</dc:date>
    </item>
  </channel>
</rss>