<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Getting started with emWin. (RamLoc64 overfloods) in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Getting-started-with-emWin-RamLoc64-overfloods/m-p/516910#M1914</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by sipel_tp on Mon May 21 11:52:25 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;Hi everybody. I need some help with emWin. I downloaded the examples for LPCXpresso v4.22 from &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fproject%2Femwin-graphics-library" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/project/emwin-graphics-library&lt;/A&gt;&lt;SPAN&gt;. The example ran perfectly using a LPC1788 Developer's Kit and a 4.3 inch (480x272 pixel) TFT LCD Display, both from Embedded Artists. After that I tried to copy the example by creating a new project using LPCXpresso wizard (the idea is to learn how to create an emWin project by myself. I imported all the needed files from the example project. I also configured some source and include paths. When I try to build the new project the compiler doesn´t complaint at all but the linker sends an error message: "RamLoc64 overfloods". I would like to know WHY this message appears and what I have to do in order to fix the problem. Thank you very much for your answers.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:23:49 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:23:49Z</dc:date>
    <item>
      <title>Getting started with emWin. (RamLoc64 overfloods)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Getting-started-with-emWin-RamLoc64-overfloods/m-p/516910#M1914</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by sipel_tp on Mon May 21 11:52:25 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;Hi everybody. I need some help with emWin. I downloaded the examples for LPCXpresso v4.22 from &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fproject%2Femwin-graphics-library" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/project/emwin-graphics-library&lt;/A&gt;&lt;SPAN&gt;. The example ran perfectly using a LPC1788 Developer's Kit and a 4.3 inch (480x272 pixel) TFT LCD Display, both from Embedded Artists. After that I tried to copy the example by creating a new project using LPCXpresso wizard (the idea is to learn how to create an emWin project by myself. I imported all the needed files from the example project. I also configured some source and include paths. When I try to build the new project the compiler doesn´t complaint at all but the linker sends an error message: "RamLoc64 overfloods". I would like to know WHY this message appears and what I have to do in order to fix the problem. Thank you very much for your answers.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:23:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Getting-started-with-emWin-RamLoc64-overfloods/m-p/516910#M1914</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:23:49Z</dc:date>
    </item>
    <item>
      <title>Re: Getting started with emWin. (RamLoc64 overfloods)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Getting-started-with-emWin-RamLoc64-overfloods/m-p/516911#M1915</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by oahmad on Tue May 22 09:47:11 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;If you are using lpcxpresso, you probably used the custom linker file that specifies a location called SDRAM32 to store 32 MEGAbytes of RAM for the frame-buffer.&amp;nbsp; In your new project, are you utilizing the same hardware?&amp;nbsp; If so, then the issue might be that you need to utilize the 'custom' linker file, not the one provided/generated an maintained by the LPCXpresso as default.&amp;nbsp; I do not use LPCXpresso, I use Code-Red, but I believe they are (were) from teh same company...in any case, in my environment, you go to the project properties, Then C/C++ Build, then under Settings, Tool Settings, In the MCU-Linker section, under Target, you need to un-check the 'Manage LInker Script' and select teh custom linker script provided for the LPCXpresso...(in my case it is "${workspace_loc:/${ProjName}/LPCXpresso406_emWin512_EA1788_320240_290911.ld}".&amp;nbsp; You also need to have the _mem.ld and _lib.ld of the same name in the same location.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:23:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Getting-started-with-emWin-RamLoc64-overfloods/m-p/516911#M1915</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:23:50Z</dc:date>
    </item>
  </channel>
</rss>