<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Custom LPC4337 PCB Feedback</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Custom-LPC4337-PCB-Feedback/m-p/574874#M19117</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wlamers on Wed Mar 27 07:46:51 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Probably a little bit late to respond, but the VBus pin already has an internal pull-down resistor. See datasheet:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;--- USB0_VBUS - I/O VBUS pin (power on USB cable). This pin includes an internal pull-down resistor of 64 k (typical)  16 k.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am not sure if you use the USB as a host. If you only use it as a device you can (or need?) to omit the 15k pull-down's also. Since these are for the host side only. The switchable 1.5k pull-up resisotrs (internal in the uC) are used to negotiate the bus speed, overruling the 15k pull-down's on the host side. See manual:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;--- USB0_DP I/O USB0 bidirectional D+ line. The D+ line has an internal 1.5 k pull-up. This pull-up is enabled when software sets the RS bit (Bit 0) in the USBCMD register and the USB0 controller sees a valid VBUS voltage&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:59:50 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:59:50Z</dc:date>
    <item>
      <title>Custom LPC4337 PCB Feedback</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Custom-LPC4337-PCB-Feedback/m-p/574869#M19112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by avr458 on Sun Mar 10 02:22:42 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;While I have been testing and debugging my first revision of my LPC4337 PCB I prepared a new design. I believe I have corrected all the design problems I had with the first one but before I send it out to be fabbed I want to make sure that I have done everything correctly and considered everything. I have attached a smart PDF exported from Altium that include my schematic and PCB (layers and composite). I want feedback on the specifics of the LPC4337 as well as feedback on my routing job/overall design. &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:59:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Custom-LPC4337-PCB-Feedback/m-p/574869#M19112</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:59:47Z</dc:date>
    </item>
    <item>
      <title>Re: Custom LPC4337 PCB Feedback</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Custom-LPC4337-PCB-Feedback/m-p/574870#M19113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wmues on Sun Mar 10 13:10:27 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;1) I am missing a Pulldown Resistor (1MOhm) at USB Device VBUS.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2) Several 1117 Voltage Regulators are instable with low ESR capacitors (ceramic) for output. Use another regulator which is specified for ceramic capacitor to avoid problems.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:59:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Custom-LPC4337-PCB-Feedback/m-p/574870#M19113</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:59:47Z</dc:date>
    </item>
    <item>
      <title>Re: Custom LPC4337 PCB Feedback</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Custom-LPC4337-PCB-Feedback/m-p/574871#M19114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by avr458 on Mon Mar 11 00:58:39 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;So I can't use that 3.3 v-reg with a ceramic cap? Which one should I use? I need 1-1.5 amps of 3.3v (its got to be able to power Arduino shields + the board).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Also why would I need a pulldown on V-bus? V-bus is just the power from the USB port, only D- and D+ are for coms and thus require pulldowns.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:59:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Custom-LPC4337-PCB-Feedback/m-p/574871#M19114</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:59:48Z</dc:date>
    </item>
    <item>
      <title>Re: Custom LPC4337 PCB Feedback</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Custom-LPC4337-PCB-Feedback/m-p/574872#M19115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wmues on Mon Mar 11 03:17:02 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I would use the 1117 with an output current of 500mA or less. If you need more output current, the 1117 will get too hot. For 1.5A, you will need a DC DC converter. Try TI TPS62063 or equivalent.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you have no Pulldown on VBUS, this pin will be floating and your software might be fooled to detect that the device is plugged over USB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:59:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Custom-LPC4337-PCB-Feedback/m-p/574872#M19115</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:59:49Z</dc:date>
    </item>
    <item>
      <title>Re: Custom LPC4337 PCB Feedback</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Custom-LPC4337-PCB-Feedback/m-p/574873#M19116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by suckfish on Tue Mar 12 11:48:55 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;It looks like you've routed the USB ID and VBUS lines very close to D+/D-.&amp;nbsp; Probably better to keep D+/D- away from other things as far as possible.&amp;nbsp; [Even better, swap the JTAG header and USB socket - that would keep the high speed USB traces much shorter.]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:59:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Custom-LPC4337-PCB-Feedback/m-p/574873#M19116</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:59:50Z</dc:date>
    </item>
    <item>
      <title>Re: Custom LPC4337 PCB Feedback</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Custom-LPC4337-PCB-Feedback/m-p/574874#M19117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wlamers on Wed Mar 27 07:46:51 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Probably a little bit late to respond, but the VBus pin already has an internal pull-down resistor. See datasheet:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;--- USB0_VBUS - I/O VBUS pin (power on USB cable). This pin includes an internal pull-down resistor of 64 k (typical)  16 k.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am not sure if you use the USB as a host. If you only use it as a device you can (or need?) to omit the 15k pull-down's also. Since these are for the host side only. The switchable 1.5k pull-up resisotrs (internal in the uC) are used to negotiate the bus speed, overruling the 15k pull-down's on the host side. See manual:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;--- USB0_DP I/O USB0 bidirectional D+ line. The D+ line has an internal 1.5 k pull-up. This pull-up is enabled when software sets the RS bit (Bit 0) in the USBCMD register and the USB0 controller sees a valid VBUS voltage&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:59:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Custom-LPC4337-PCB-Feedback/m-p/574874#M19117</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:59:50Z</dc:date>
    </item>
  </channel>
</rss>