<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPCScrypt operation with Code Protect CRP1 enabled</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-operation-with-Code-Protect-CRP1-enabled/m-p/574564#M19056</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With CRP set to CRP1 or higher, available boot sources are restricted: If the requested boot source (either hardwired boot source from OTP or read from pins) is not one of UART0/UART3, the boot code forces booting from UART0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So there is no way to boot into USB DFU mode (as required by LPCScrypt) on a CRP protected device. You will have to unlock over the UART using Flashmagic or similar first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Aug 2016 10:20:51 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2016-08-11T10:20:51Z</dc:date>
    <item>
      <title>LPCScrypt operation with Code Protect CRP1 enabled</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-operation-with-Code-Protect-CRP1-enabled/m-p/574563#M19055</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Will LPCScrypt work when code protection CRP1 is enabled. It appears to break the ability to run LPCScrypt by preventing the LPC1833 being detected as a USB device/COM port.&lt;/P&gt;&lt;P&gt;If this is the case, how can we Erase the Device (allowed in CRP1), so that LPC Scrypt will work again?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Aug 2016 11:22:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-operation-with-Code-Protect-CRP1-enabled/m-p/574563#M19055</guid>
      <dc:creator>gileshutchison</dc:creator>
      <dc:date>2016-08-05T11:22:02Z</dc:date>
    </item>
    <item>
      <title>Re: LPCScrypt operation with Code Protect CRP1 enabled</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-operation-with-Code-Protect-CRP1-enabled/m-p/574564#M19056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With CRP set to CRP1 or higher, available boot sources are restricted: If the requested boot source (either hardwired boot source from OTP or read from pins) is not one of UART0/UART3, the boot code forces booting from UART0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So there is no way to boot into USB DFU mode (as required by LPCScrypt) on a CRP protected device. You will have to unlock over the UART using Flashmagic or similar first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 10:20:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-operation-with-Code-Protect-CRP1-enabled/m-p/574564#M19056</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-08-11T10:20:51Z</dc:date>
    </item>
  </channel>
</rss>