<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PLL in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/PLL/m-p/574349#M19014</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Dilberto on Sat Mar 01 07:32:39 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;What is the max frequency of LPC-812 Board?&lt;BR /&gt;What is the max frequency of pll ?&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;According to NxP doc UM10601 ( LPC800 User manual, Rev. 1.3 — 22 July 2013 ) :&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;The input frequency range is 10 MHz to 25 MHz.&lt;BR /&gt;The CCO frequency range is 156 MHz to 320 MHz.&lt;BR /&gt;Remark: The divider values for P and M must be selected so that the PLL output clock&lt;BR /&gt;frequency FCLKOUT is lower than 100 MHz because the main clock is limited to a&lt;BR /&gt;maximum frequency of 100 MHz&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Kindly remember that, in the LPC812-Max Board, the crystal, although present in the board, is NOT wired to the microcontroller.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This can be done by changing jumpers SJ2 and SJ3 ( see attached figure ).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The processor can run with CPU clock up to 30 MHz without introducing wait states ( see Flash Memory Controller ( FMC ) register set, pg 260 of referred manual ).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Above this value and up to 100 MHz, wait states must be introduced for memory access.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However, beware of the power consumption! As higher the frequency used, higher the power consumption is.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Hope this helps.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 20:14:34 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T20:14:34Z</dc:date>
    <item>
      <title>PLL</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/PLL/m-p/574348#M19013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by vijay_nav on Sat Mar 01 00:23:31 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;What is the max frequency of LPC-812 Board?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What is the max frequency of pll ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;can we use PLL to LPC-812 board.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:14:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/PLL/m-p/574348#M19013</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:14:34Z</dc:date>
    </item>
    <item>
      <title>Re: PLL</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/PLL/m-p/574349#M19014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Dilberto on Sat Mar 01 07:32:39 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;What is the max frequency of LPC-812 Board?&lt;BR /&gt;What is the max frequency of pll ?&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;According to NxP doc UM10601 ( LPC800 User manual, Rev. 1.3 — 22 July 2013 ) :&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;The input frequency range is 10 MHz to 25 MHz.&lt;BR /&gt;The CCO frequency range is 156 MHz to 320 MHz.&lt;BR /&gt;Remark: The divider values for P and M must be selected so that the PLL output clock&lt;BR /&gt;frequency FCLKOUT is lower than 100 MHz because the main clock is limited to a&lt;BR /&gt;maximum frequency of 100 MHz&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Kindly remember that, in the LPC812-Max Board, the crystal, although present in the board, is NOT wired to the microcontroller.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This can be done by changing jumpers SJ2 and SJ3 ( see attached figure ).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The processor can run with CPU clock up to 30 MHz without introducing wait states ( see Flash Memory Controller ( FMC ) register set, pg 260 of referred manual ).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Above this value and up to 100 MHz, wait states must be introduced for memory access.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However, beware of the power consumption! As higher the frequency used, higher the power consumption is.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Hope this helps.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:14:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/PLL/m-p/574349#M19014</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:14:34Z</dc:date>
    </item>
  </channel>
</rss>