<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックQuestion about the bandwidth test app</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Question-about-the-bandwidth-test-app/m-p/516847#M1878</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cgha on Fri Nov 23 01:20:04 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to test the LPC1768 board usb bandwidth in bulk mode, but the firmware project is using LPCXpresso IDE, so I just use a general usb bulk prject that I migrate from keil mdk and it use keil usb stack , and I use libusb-win inf-wizard create the driver file, tested with libusb bulk example, it works. But the problem is When I try to use the LPCUsbTest in the bandwidth test project, it can not find my device even I changed the guid in the project(I just copy the guid from inf file and replaced the guid defined in LPCDISPLAY_GUID_STRING). So what should I do if I want to do the test?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;ChrisChen&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:26:28 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:26:28Z</dc:date>
    <item>
      <title>Question about the bandwidth test app</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Question-about-the-bandwidth-test-app/m-p/516847#M1878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cgha on Fri Nov 23 01:20:04 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to test the LPC1768 board usb bandwidth in bulk mode, but the firmware project is using LPCXpresso IDE, so I just use a general usb bulk prject that I migrate from keil mdk and it use keil usb stack , and I use libusb-win inf-wizard create the driver file, tested with libusb bulk example, it works. But the problem is When I try to use the LPCUsbTest in the bandwidth test project, it can not find my device even I changed the guid in the project(I just copy the guid from inf file and replaced the guid defined in LPCDISPLAY_GUID_STRING). So what should I do if I want to do the test?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;ChrisChen&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:26:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Question-about-the-bandwidth-test-app/m-p/516847#M1878</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:26:28Z</dc:date>
    </item>
    <item>
      <title>Re: Question about the bandwidth test app</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Question-about-the-bandwidth-test-app/m-p/516848#M1879</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nxpUSBlib team on Tue Nov 27 17:29:45 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Are you talking about the new Project_BandwidthTest project in the latest release (v0.98a) of nxpUSBlib? If so, you should be able to recreate the firmware using the Keil stack as long as you make it a Vendor Specific class device and use the same VID/PID.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also, to use the WinUSB test app in Windows you will need to install using the .inf file from the download on lpcware.com. Did you do this installation?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:26:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Question-about-the-bandwidth-test-app/m-p/516848#M1879</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:26:29Z</dc:date>
    </item>
  </channel>
</rss>