<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックIBIS model for lpc1788, choosing the correct PIN model for EMC pins.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-model-for-lpc1788-choosing-the-correct-PIN-model-for-EMC/m-p/516829#M1877</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jborge on Mon Jul 27 10:49:57 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;lpc1788 208lqfp interfacing to IS42S32800D-7TL-TR&amp;nbsp; SDRAM memory.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have installed the IBIS models for the LPC1788 and the ISS SDRAM in ALTIUM designer for PCB waveform simulation..&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When simulating I noticed the edge rates on the data lines from the SDRAM to the LPC1788 to be within reason for risetimes on the wave forms. I observe the expected overshoot, undershoot as I would expect to see.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When looking at waveforms for LPC1788 EMC pins, for example the CLK and DATA they seem to be heavily slewed.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So data wave forms going from the SDRAM to the LPC1788 have expected risetimes and data signals going from the LPC1788 to the SDRAM and heavily slewed waveforms. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;There are several models:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;for example:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;out_2.5v_tp_out.mac&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;out_2.5v_st_out.mac&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;plus several more.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What IO model should I select for the CLK output, and memory outputs for the EMC pins?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also I noticed that IBIS file for the LPC1788 does not load well into a text editor for viewing. It seem to be missing all the form feed and CR characters.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Where as the IBIS model for other components for example the lpc1850 and the SDRAM used above can easily be viewed and studied in a text editor.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance for any replies.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:23:41 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:23:41Z</dc:date>
    <item>
      <title>IBIS model for lpc1788, choosing the correct PIN model for EMC pins.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-model-for-lpc1788-choosing-the-correct-PIN-model-for-EMC/m-p/516829#M1877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jborge on Mon Jul 27 10:49:57 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;lpc1788 208lqfp interfacing to IS42S32800D-7TL-TR&amp;nbsp; SDRAM memory.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have installed the IBIS models for the LPC1788 and the ISS SDRAM in ALTIUM designer for PCB waveform simulation..&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When simulating I noticed the edge rates on the data lines from the SDRAM to the LPC1788 to be within reason for risetimes on the wave forms. I observe the expected overshoot, undershoot as I would expect to see.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When looking at waveforms for LPC1788 EMC pins, for example the CLK and DATA they seem to be heavily slewed.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So data wave forms going from the SDRAM to the LPC1788 have expected risetimes and data signals going from the LPC1788 to the SDRAM and heavily slewed waveforms. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;There are several models:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;for example:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;out_2.5v_tp_out.mac&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;out_2.5v_st_out.mac&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;plus several more.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What IO model should I select for the CLK output, and memory outputs for the EMC pins?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also I noticed that IBIS file for the LPC1788 does not load well into a text editor for viewing. It seem to be missing all the form feed and CR characters.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Where as the IBIS model for other components for example the lpc1850 and the SDRAM used above can easily be viewed and studied in a text editor.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance for any replies.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:23:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/IBIS-model-for-lpc1788-choosing-the-correct-PIN-model-for-EMC/m-p/516829#M1877</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:23:41Z</dc:date>
    </item>
  </channel>
</rss>