<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックHi, I am using LPC 3250 controller and though able to enter stop mode the processor is not returning to Run mode even after doing register settings. i want processor to wake up when a GPI interrupt occurs. Please help in this and share some sample codes.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hi-I-am-using-LPC-3250-controller-and-though-able-to-enter-stop/m-p/573027#M18703</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the system, LPC 3250 is running in RUN mode and when the processor is idle, it should enter stop mode and then on occurrence of a GPI interrupt, it should return to RUN mode. Though instructions in User manual were followed required result didn't come, So please give some idea and details how to achieve this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Jul 2016 05:28:33 GMT</pubDate>
    <dc:creator>vikhyathkumar</dc:creator>
    <dc:date>2016-07-15T05:28:33Z</dc:date>
    <item>
      <title>Hi, I am using LPC 3250 controller and though able to enter stop mode the processor is not returning to Run mode even after doing register settings. i want processor to wake up when a GPI interrupt occurs. Please help in this and share some sample codes.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hi-I-am-using-LPC-3250-controller-and-though-able-to-enter-stop/m-p/573027#M18703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the system, LPC 3250 is running in RUN mode and when the processor is idle, it should enter stop mode and then on occurrence of a GPI interrupt, it should return to RUN mode. Though instructions in User manual were followed required result didn't come, So please give some idea and details how to achieve this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jul 2016 05:28:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Hi-I-am-using-LPC-3250-controller-and-though-able-to-enter-stop/m-p/573027#M18703</guid>
      <dc:creator>vikhyathkumar</dc:creator>
      <dc:date>2016-07-15T05:28:33Z</dc:date>
    </item>
    <item>
      <title>Re: Hi, I am using LPC 3250 controller and though able to enter stop mode the processor is not returning to Run mode even after doing register settings. i want processor to wake up when a GPI interrupt occurs. Please help in this and share some sample cod</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hi-I-am-using-LPC-3250-controller-and-though-able-to-enter-stop/m-p/573028#M18704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; Vikhyath,&lt;/P&gt;&lt;P&gt;I was wondering if you can answer there questions below.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Did the current consumption reduce after execute the enter the stop mode function?&lt;/LI&gt;&lt;LI&gt;After the MCU executes the enter the stop mode function, what's the next status of the MCU, for instance the MCU can still runs or just break down.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2016 03:16:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Hi-I-am-using-LPC-3250-controller-and-though-able-to-enter-stop/m-p/573028#M18704</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-07-20T03:16:32Z</dc:date>
    </item>
  </channel>
</rss>