<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Maximum USART Baud Rate on LPC43xx (&amp;gt; 15 Mbit/s ?)</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Maximum-USART-Baud-Rate-on-LPC43xx-gt-15-Mbit-s/m-p/572661#M18629</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by eamonnh on Fri Aug 08 03:02:06 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Scottreed,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I've run comms between a pair of 43xx at 51MHz using an oversampling ratio of 4. Seemed rock-solid. However, I think a ratio of 6 is preferable for more robustness and reliability. Even Uart1 has an OSR register even though it's not declared in the docs. I often use Uart1 as a console @ 3MHz driven from the 12MHz IRC, with oversample of 4. (Allows me to change CPU frequency freely without having to worry about console.)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I believe that anything from 34MHz down is pretty robust but it would need testing in your application to see if the waveforms arrive sufficiently undistorted to deliver reliable comms.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The NXP UARTs are really well-engineered peripherals.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Kind regards - Eamonn&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:57:00 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:57:00Z</dc:date>
    <item>
      <title>Maximum USART Baud Rate on LPC43xx (&gt; 15 Mbit/s ?)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Maximum-USART-Baud-Rate-on-LPC43xx-gt-15-Mbit-s/m-p/572660#M18628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Scottreed on Thu Aug 07 20:29:30 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;According to the datasheet, the maximum USART Baud Rate on LPC43xx is 8 Mbit/s.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However, it could be 12.75Mbit/s in following thread&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fforum%2Fusart-baudrate-8-mbit-204mhz" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/forum/usart-baudrate-8-mbit-204mhz&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I need 16 Mbit/s or more for my application.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;On the page 1116 of user manual UM10503, the default OSINT (Integer part of oversampling ratio) is 16. Can I just change it to 8 for 16 Mbit/s baud rate?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Mostly, x8 oversampling is already very reliable.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance,&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:56:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Maximum-USART-Baud-Rate-on-LPC43xx-gt-15-Mbit-s/m-p/572660#M18628</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:56:59Z</dc:date>
    </item>
    <item>
      <title>Re: Maximum USART Baud Rate on LPC43xx (&gt; 15 Mbit/s ?)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Maximum-USART-Baud-Rate-on-LPC43xx-gt-15-Mbit-s/m-p/572661#M18629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by eamonnh on Fri Aug 08 03:02:06 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Scottreed,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I've run comms between a pair of 43xx at 51MHz using an oversampling ratio of 4. Seemed rock-solid. However, I think a ratio of 6 is preferable for more robustness and reliability. Even Uart1 has an OSR register even though it's not declared in the docs. I often use Uart1 as a console @ 3MHz driven from the 12MHz IRC, with oversample of 4. (Allows me to change CPU frequency freely without having to worry about console.)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I believe that anything from 34MHz down is pretty robust but it would need testing in your application to see if the waveforms arrive sufficiently undistorted to deliver reliable comms.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The NXP UARTs are really well-engineered peripherals.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Kind regards - Eamonn&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:57:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Maximum-USART-Baud-Rate-on-LPC43xx-gt-15-Mbit-s/m-p/572661#M18629</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:57:00Z</dc:date>
    </item>
  </channel>
</rss>