<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC7399 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC7399/m-p/572628#M18626</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Pacman on Mon Oct 06 21:45:55 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;If you want to go beyond 400MHz, the microcontroller will cost a lot more.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This is because the 28nm will go up to 400MHz, but of course if you're speaking about 10nm technology, you'll be able to get past the 400MHz limit. ;)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-We'll need to keep the price of the M7 below the A5 too. :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm pretty confident that you would be able to do 400M memory operations per second with the 400MHz Cortex-M7, because it has a dual ALU.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;SRAM: Agree: More SRAM. 512kB if possible - and contigous. I don't care about Flash memory, as long as there's more than 8kB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Flash memory isn't really important for me.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It's possible to run high-speed subroutines from SRAM; which is impossible to do in Flash, due to the delay.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So 3MB Flash memory is way over my needs (I don't need to install Windows or put uncompressed pictures in there).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'd prefer having 8kB Flash and then 256kB or 512kB SRAM compared to 4MB Flash and 240kB SRAM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-Because I can always interface external memory (such as SPI, SPIFI, SD/MMC, NAND or NOR) without losing much speed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The speed will be gained back when copying a routine to SRAM temporarily and throwing it away after use.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note: I'm not saying that there should be no Flash memory at all. I'm just emphasizing how important SRAM is to me.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I would not mind having 128kB Flash memory or more.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;DACS: Agree, but I'd prefer 6 of them.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;And as JohnR says ... SGPIO should have an option for lsb/msb first, plus an extra option for byte-reversing (4 combinations)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(perhaps being able to control each SGPIO line's bit stream individually, in order to allow multiple interface types at the same time)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Enhanced DMA would be real cool [eg. repeat-count with interleave-increment for each transfer on both source and destination, so you wouldn't have to have 500+ LLIs], but as this is ARM's technology, it's ARM that needs to enhance it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes, and dual logical (AND/OR/XOR) operations on each DMA transfer too one for first transfer, one for next N transfers and one for the last transfer - on both source and destination - I know, I know, I'm asking for too much here.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:56:59 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:56:59Z</dc:date>
    <item>
      <title>LPC7399</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC7399/m-p/572624#M18622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by hlsa on Wed Sep 24 05:48:19 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;After reading abou the new ARM Cortex M7 yesterday, I am looking forward to get the LPC7399. Here some technical details:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]Quad core MCU with one M7 core and three M0 cores running at 300 MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]3 MB integrated Flash Memory&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]Dedicated Crc unit for Hardware based CRC16 / CRC32 calculations.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]32 channel DMA Controller&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]4 U(S)ART Interfaces @ 20 MBit/s &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]Other peripherals similar to LPC4357&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Oops. Just a dream.&amp;nbsp; ;-) ... But maybe it is good to give NXP some time to develop it properly (nothing worse than a lot of errata).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:56:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC7399/m-p/572624#M18622</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:56:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPC7399</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC7399/m-p/572625#M18623</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Benjamin Vernoux on Wed Sep 24 15:10:11 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC7xxx DualCore Cortex M7 min @400MHz (and up to 800MHz) + 1 M0+ for peripherals with following features:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- An updated dual SGPIO (up to Dual 16bits + Clocks) to offer 12 an 16bits !! instead of a limitation to 8bits mode in order to interface with a modern 16bits DAC + 16bits ADC &amp;gt; 20MSPS&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- ADC HS 20MSPS 16bits (or 40MSPS 12bits) including configurable hardware decimation and filter.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- DAC HS 80MSPS 16bits.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Dual Hardware FIFO peripheral with configurable addr+size in SRAM/SDRAM area + DMA.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Ethernet Gigabit with HW ip/udp packet+crc (will be a must for realtime data).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Dual integrated USB 2.0 HS PHY (instead of having only 1 integrated HS PHY).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- USB3.1 Device, even if it is limited by the bus/mcu to something like 200Mbytes/s will be a must for realtime data.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- More SRAM (512KB total will be a must) + more banks on different dedicated bus.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:56:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC7399/m-p/572625#M18623</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:56:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPC7399</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC7399/m-p/572626#M18624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by JohnR on Thu Sep 25 05:50:35 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt; An updated dual SGPIO (up to Dual 16bits + Clocks) to offer 12 an 16bits !! instead of a limitation to 8bits mode in order to interface with a modern 16bits DAC + 16bits ADC &amp;gt; 20MSPS&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Add the ability tor reverse the direction of the shift registers to accommodate both MSB and LSB serial data.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;John.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:56:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC7399/m-p/572626#M18624</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:56:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPC7399</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC7399/m-p/572627#M18625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rocketdawg on Sun Oct 05 12:58:07 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Benjamin Vernoux&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;LPC7xxx DualCore Cortex M7 min @400MHz (and up to 800MHz) + 1 M0+ for peripherals with following features:&lt;BR /&gt;- ADC HS 20MSPS 16bits (or 40MSPS 12bits) including configurable hardware decimation and filter.&lt;BR /&gt;- DAC HS 80MSPS 16bits.&lt;BR /&gt;- More SRAM (512KB total will be a must) + more banks on different dedicated bus.&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;drop the M0+.&amp;nbsp; Have parts that add a optional M3, or M4.&amp;nbsp; Vybrid does an A5/M4.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Since the LPC4370 already does 80 MSPS ADC, I would say that is a minimum.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PIC32MZ has 512K RAM, but it is so damaged by errata.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and make some of the RAM more contiguous.&amp;nbsp; The LPC43xx memory map is a bit disjointed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:56:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC7399/m-p/572627#M18625</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:56:58Z</dc:date>
    </item>
    <item>
      <title>Re: LPC7399</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC7399/m-p/572628#M18626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Pacman on Mon Oct 06 21:45:55 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;If you want to go beyond 400MHz, the microcontroller will cost a lot more.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This is because the 28nm will go up to 400MHz, but of course if you're speaking about 10nm technology, you'll be able to get past the 400MHz limit. ;)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-We'll need to keep the price of the M7 below the A5 too. :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm pretty confident that you would be able to do 400M memory operations per second with the 400MHz Cortex-M7, because it has a dual ALU.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;SRAM: Agree: More SRAM. 512kB if possible - and contigous. I don't care about Flash memory, as long as there's more than 8kB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Flash memory isn't really important for me.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It's possible to run high-speed subroutines from SRAM; which is impossible to do in Flash, due to the delay.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So 3MB Flash memory is way over my needs (I don't need to install Windows or put uncompressed pictures in there).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'd prefer having 8kB Flash and then 256kB or 512kB SRAM compared to 4MB Flash and 240kB SRAM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-Because I can always interface external memory (such as SPI, SPIFI, SD/MMC, NAND or NOR) without losing much speed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The speed will be gained back when copying a routine to SRAM temporarily and throwing it away after use.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note: I'm not saying that there should be no Flash memory at all. I'm just emphasizing how important SRAM is to me.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I would not mind having 128kB Flash memory or more.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;DACS: Agree, but I'd prefer 6 of them.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;And as JohnR says ... SGPIO should have an option for lsb/msb first, plus an extra option for byte-reversing (4 combinations)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(perhaps being able to control each SGPIO line's bit stream individually, in order to allow multiple interface types at the same time)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Enhanced DMA would be real cool [eg. repeat-count with interleave-increment for each transfer on both source and destination, so you wouldn't have to have 500+ LLIs], but as this is ARM's technology, it's ARM that needs to enhance it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes, and dual logical (AND/OR/XOR) operations on each DMA transfer too one for first transfer, one for next N transfers and one for the last transfer - on both source and destination - I know, I know, I'm asking for too much here.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:56:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC7399/m-p/572628#M18626</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:56:59Z</dc:date>
    </item>
  </channel>
</rss>