<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem Using all I2C Ports on LPC824 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-Using-all-I2C-Ports-on-LPC824/m-p/571905#M18484</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by FirmLogic on Wed Dec 03 10:03:55 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC824-MAX board ... &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I expanded the sample code for file "periph_i2cm_interrupt" to setup and use all I2C ports in interrupt mode.&amp;nbsp; (LPCOpen does not provide sample code for the non fixed I2C port.) Only I2C0 causes an interrupt. I get no activity on the other I2C ports.&amp;nbsp; I studied the user manual in effort to determine what possible step I am missing. When debugging, after loading the MSTDAT register and the start command in the MSTCTL register, the STAT register is always "0".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there a sample code for seting up the other I2C ports?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 20:11:35 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T20:11:35Z</dc:date>
    <item>
      <title>Problem Using all I2C Ports on LPC824</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-Using-all-I2C-Ports-on-LPC824/m-p/571905#M18484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by FirmLogic on Wed Dec 03 10:03:55 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC824-MAX board ... &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I expanded the sample code for file "periph_i2cm_interrupt" to setup and use all I2C ports in interrupt mode.&amp;nbsp; (LPCOpen does not provide sample code for the non fixed I2C port.) Only I2C0 causes an interrupt. I get no activity on the other I2C ports.&amp;nbsp; I studied the user manual in effort to determine what possible step I am missing. When debugging, after loading the MSTDAT register and the start command in the MSTCTL register, the STAT register is always "0".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there a sample code for seting up the other I2C ports?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:11:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-Using-all-I2C-Ports-on-LPC824/m-p/571905#M18484</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:11:35Z</dc:date>
    </item>
    <item>
      <title>Re: Problem Using all I2C Ports on LPC824</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-Using-all-I2C-Ports-on-LPC824/m-p/571906#M18485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by FirmLogic on Wed Dec 31 22:00:56 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Problem was solved: Had to drop the LPC824 MAX board driver library which was always enabling all fixed functions which was overriding my setup.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:11:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-Using-all-I2C-Ports-on-LPC824/m-p/571906#M18485</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:11:36Z</dc:date>
    </item>
  </channel>
</rss>