<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC800 ISP connect  in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC800-ISP-connect/m-p/568939#M17816</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheShed on Fri Mar 01 04:45:08 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Not a great piece of design is it.... &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;With the trimming pot wound all the way up the external uart can never pull ISP-RX below half rail. In my setup it doesn't get much below 1.9V which is well outside the limit for a valid LOW of 0.3VDD. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;On the plus side, it is a 22k pot so set it to anywhere *except* against the end stop and it should be fine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I think this highlights the one flaw I have found so far with the LPC8xx design: The two analogue compare inputs are both assigned to ISP pins. One would have been OK but not both.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could I request that this is changed for the next part in the family - please...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;--&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;mike&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 20:11:01 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T20:11:01Z</dc:date>
    <item>
      <title>LPC800 ISP connect</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC800-ISP-connect/m-p/568938#M17815</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by idol on Fri Mar 01 02:30:31 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;when&amp;nbsp; we connect the isp&amp;nbsp; of lpcxpresso LPC812, We must pay attention to R55 that is connected to AD.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;We must put the resistance welding down,or we cannot connect the isp&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:11:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC800-ISP-connect/m-p/568938#M17815</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:11:01Z</dc:date>
    </item>
    <item>
      <title>Re: LPC800 ISP connect</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC800-ISP-connect/m-p/568939#M17816</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheShed on Fri Mar 01 04:45:08 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Not a great piece of design is it.... &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;With the trimming pot wound all the way up the external uart can never pull ISP-RX below half rail. In my setup it doesn't get much below 1.9V which is well outside the limit for a valid LOW of 0.3VDD. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;On the plus side, it is a 22k pot so set it to anywhere *except* against the end stop and it should be fine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I think this highlights the one flaw I have found so far with the LPC8xx design: The two analogue compare inputs are both assigned to ISP pins. One would have been OK but not both.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could I request that this is changed for the next part in the family - please...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;--&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;mike&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:11:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC800-ISP-connect/m-p/568939#M17816</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:11:01Z</dc:date>
    </item>
  </channel>
</rss>