<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックQuestion on User Manual Rev. 1 - 12 Nov 2012: Page 8 Footnote 3: Do not use this pads for high-speed application such as SPI...</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Question-on-User-Manual-Rev-1-12-Nov-2012-Page-8-Footnote-3-Do/m-p/568905#M17810</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by capiman on Tue Feb 19 02:12:55 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a question regarding User Manual Rev. 1 - 12 Nov 2012: &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;On page 8 there is footnote 3: "Do not use this pads for high-speed application such as SPI or USART".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Are the pads PIO0_10 and PIO0_11 not useable at all for SPI or USART?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Or are they useable, but due to electrical characteristic (e.g. filters, ...), but only for low speed of SPI or USART?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If yes, what is the speed limit? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is RS232 e.g. with 115200 or SPI with 400 kHz possible, because it is in the same range as I2C?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 20:10:50 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T20:10:50Z</dc:date>
    <item>
      <title>Question on User Manual Rev. 1 - 12 Nov 2012: Page 8 Footnote 3: Do not use this pads for high-speed application such as SPI...</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Question-on-User-Manual-Rev-1-12-Nov-2012-Page-8-Footnote-3-Do/m-p/568905#M17810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by capiman on Tue Feb 19 02:12:55 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a question regarding User Manual Rev. 1 - 12 Nov 2012: &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;On page 8 there is footnote 3: "Do not use this pads for high-speed application such as SPI or USART".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Are the pads PIO0_10 and PIO0_11 not useable at all for SPI or USART?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Or are they useable, but due to electrical characteristic (e.g. filters, ...), but only for low speed of SPI or USART?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If yes, what is the speed limit? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is RS232 e.g. with 115200 or SPI with 400 kHz possible, because it is in the same range as I2C?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:10:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Question-on-User-Manual-Rev-1-12-Nov-2012-Page-8-Footnote-3-Do/m-p/568905#M17810</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:10:50Z</dc:date>
    </item>
    <item>
      <title>Re: Question on User Manual Rev. 1 - 12 Nov 2012: Page 8 Footnote 3: Do not use this pads for high-speed application such as SPI...</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Question-on-User-Manual-Rev-1-12-Nov-2012-Page-8-Footnote-3-Do/m-p/568906#M17811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by capiman on Tue Feb 19 07:07:57 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Correction of my question: The footnote 3 is not in User Manual, but in Objective data sheet.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;BTW: Same text in Objective data sheet Rev. 2 - 28 January 2013.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:10:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Question-on-User-Manual-Rev-1-12-Nov-2012-Page-8-Footnote-3-Do/m-p/568906#M17811</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:10:51Z</dc:date>
    </item>
    <item>
      <title>Re: Question on User Manual Rev. 1 - 12 Nov 2012: Page 8 Footnote 3: Do not use this pads for high-speed application such as SPI...</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Question-on-User-Manual-Rev-1-12-Nov-2012-Page-8-Footnote-3-Do/m-p/568907#M17812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Wouter on Thu Feb 21 00:22:29 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Capiman,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;PIO0_10 and PIO0_11 on the LPC800 are true open-drain outputs. When configured as an output, they require a pull-up resistor to set the pin high. The maximum speed will depend on the value of this pull-up resistor, and the loading on the pin. An UART @ 115200 baud or SPI at 400KHz should be no problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Wouter&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:10:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Question-on-User-Manual-Rev-1-12-Nov-2012-Page-8-Footnote-3-Do/m-p/568907#M17812</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:10:52Z</dc:date>
    </item>
  </channel>
</rss>