<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 I2C library to pressure sensor</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/I2C-library-to-pressure-sensor/m-p/568509#M17739</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mc1992 on Sat Jan 30 17:22:20 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello friends!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using a sensor of pressure, this used I2C as a means of comunication. I want to use the library i2c_18xx_43xx.h of lpcopen.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The following functions are sufficient for reading and writing to the sensor ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;--&amp;gt;Chip_I2C_Init(I2C_ID_T id);&lt;BR /&gt;--&amp;gt;Chip_I2C_SetClockRate(I2C_ID_T id, uint32_t clockrate);&lt;BR /&gt;--&amp;gt;Chip_I2C_MasterSend(I2C_ID_T id, uint8_t slaveAddr, const uint8_t *buff, uint8_t len);&lt;BR /&gt;--&amp;gt;Chip_I2C_MasterRead(I2C_ID_T id, uint8_t slaveAddr, uint8_t *buff, int len);&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!!!!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:52:02 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:52:02Z</dc:date>
    <item>
      <title>I2C library to pressure sensor</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/I2C-library-to-pressure-sensor/m-p/568509#M17739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mc1992 on Sat Jan 30 17:22:20 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello friends!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using a sensor of pressure, this used I2C as a means of comunication. I want to use the library i2c_18xx_43xx.h of lpcopen.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The following functions are sufficient for reading and writing to the sensor ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;--&amp;gt;Chip_I2C_Init(I2C_ID_T id);&lt;BR /&gt;--&amp;gt;Chip_I2C_SetClockRate(I2C_ID_T id, uint32_t clockrate);&lt;BR /&gt;--&amp;gt;Chip_I2C_MasterSend(I2C_ID_T id, uint8_t slaveAddr, const uint8_t *buff, uint8_t len);&lt;BR /&gt;--&amp;gt;Chip_I2C_MasterRead(I2C_ID_T id, uint8_t slaveAddr, uint8_t *buff, int len);&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!!!!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:52:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/I2C-library-to-pressure-sensor/m-p/568509#M17739</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:52:02Z</dc:date>
    </item>
  </channel>
</rss>