<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 SPI on LPC-Link 2 (OM13054) Header J3</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SPI-on-LPC-Link-2-OM13054-Header-J3/m-p/567237#M17488</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by OllieK on Mon Jan 06 18:21:16 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This &lt;/SPAN&gt;&lt;STRONG&gt;LPC4370&lt;/STRONG&gt;&lt;SPAN&gt; based board has one Synchronous Serial Port (&lt;/SPAN&gt;&lt;STRONG&gt;SSP1&lt;/STRONG&gt;&lt;SPAN&gt;) connected to &lt;/SPAN&gt;&lt;STRONG&gt;J3 &lt;/STRONG&gt;&lt;SPAN&gt;together with UART2, I2C, GPI05_8, GPI03_5, GPIO05_9, and GPI03_7.&amp;nbsp; There is only one SSP_SEL signal (pin 6).&amp;nbsp; In my application, there are multiple SPI slaves.&amp;nbsp;&amp;nbsp; The questions are:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1) Can I use the GPIO signals in this connector for slave selection&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2) What is the difference between the SSP_SEL and the GPIO signals&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3) What is (are) the SPI libraries to be used for multi-slave configuration&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4) Is the mutli-slave configuration supported by FreeRtos&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;5) Is the multi-slave configuration supported by DMA&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:53:02 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:53:02Z</dc:date>
    <item>
      <title>SPI on LPC-Link 2 (OM13054) Header J3</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SPI-on-LPC-Link-2-OM13054-Header-J3/m-p/567237#M17488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by OllieK on Mon Jan 06 18:21:16 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This &lt;/SPAN&gt;&lt;STRONG&gt;LPC4370&lt;/STRONG&gt;&lt;SPAN&gt; based board has one Synchronous Serial Port (&lt;/SPAN&gt;&lt;STRONG&gt;SSP1&lt;/STRONG&gt;&lt;SPAN&gt;) connected to &lt;/SPAN&gt;&lt;STRONG&gt;J3 &lt;/STRONG&gt;&lt;SPAN&gt;together with UART2, I2C, GPI05_8, GPI03_5, GPIO05_9, and GPI03_7.&amp;nbsp; There is only one SSP_SEL signal (pin 6).&amp;nbsp; In my application, there are multiple SPI slaves.&amp;nbsp;&amp;nbsp; The questions are:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1) Can I use the GPIO signals in this connector for slave selection&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2) What is the difference between the SSP_SEL and the GPIO signals&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3) What is (are) the SPI libraries to be used for multi-slave configuration&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4) Is the mutli-slave configuration supported by FreeRtos&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;5) Is the multi-slave configuration supported by DMA&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:53:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SPI-on-LPC-Link-2-OM13054-Header-J3/m-p/567237#M17488</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:53:02Z</dc:date>
    </item>
  </channel>
</rss>