<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC 822 ISP Write to RAM echoes correctly, but OK response never received!</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-822-ISP-Write-to-RAM-echoes-correctly-but-OK-response-never/m-p/567133#M17469</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Same here on a LPC15xx. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;work around:&lt;/P&gt;&lt;P&gt;I verify the complete download with the ‘Read CRC checksum’ which is described in UM10736.&lt;/P&gt;&lt;P&gt;This could also be done with fractions on the ram address or related flash address after ‘Copy RAM to flash’.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Jul 2017 15:13:39 GMT</pubDate>
    <dc:creator>andreasschnitze</dc:creator>
    <dc:date>2017-07-06T15:13:39Z</dc:date>
    <item>
      <title>LPC 822 ISP Write to RAM echoes correctly, but OK response never received!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-822-ISP-Write-to-RAM-echoes-correctly-but-OK-response-never/m-p/567131#M17467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by schoeler on Mon Apr 11 17:39:15 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;According to 25.6.1.4 of LPC82X_UM10800, after a command with an acceptable address, length, and count is received, the LPC will respond with CMD_SUCCESS ("0").&amp;nbsp; At this point, the host then sends a length amount of bytes, and the LPC should respond with "OK&amp;lt;CR&amp;gt;&amp;lt;LF&amp;gt;".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;There have been some instances of the OK&amp;lt;CR&amp;gt;&amp;lt;LF&amp;gt; not occuring, but no confirmation from NXP (for example, &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fforum%2Ferror-isp-lpc812-lost-characters-when-sending-bytes-too-fast-lpc812-command-w%23comment-1145095" rel="nofollow" target="_blank"&gt;https://www.lpcware.com/content/forum/error-isp-lpc812-lost-characters-when-sending-bytes-too-fast-lpc812-command-w#comment-1145095&lt;/A&gt;&lt;SPAN&gt; comment 14).&amp;nbsp; This is not listed in the Errata sheet Rev 1.1.&amp;nbsp; &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has anyone else seen this issue?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Even though there is no return code, a READ from the same location returns all the values I have sent.&amp;nbsp; So I know the data is in RAM, but there just seems to be no return code, contrary to what is stated in the manual.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:09:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-822-ISP-Write-to-RAM-echoes-correctly-but-OK-response-never/m-p/567131#M17467</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:09:27Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 822 ISP Write to RAM echoes correctly, but OK response never received!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-822-ISP-Write-to-RAM-echoes-correctly-but-OK-response-never/m-p/567132#M17468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jun 2016 01:07:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-822-ISP-Write-to-RAM-echoes-correctly-but-OK-response-never/m-p/567132#M17468</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-19T01:07:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 822 ISP Write to RAM echoes correctly, but OK response never received!</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-822-ISP-Write-to-RAM-echoes-correctly-but-OK-response-never/m-p/567133#M17469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Same here on a LPC15xx. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;work around:&lt;/P&gt;&lt;P&gt;I verify the complete download with the ‘Read CRC checksum’ which is described in UM10736.&lt;/P&gt;&lt;P&gt;This could also be done with fractions on the ram address or related flash address after ‘Copy RAM to flash’.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 15:13:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-822-ISP-Write-to-RAM-echoes-correctly-but-OK-response-never/m-p/567133#M17469</guid>
      <dc:creator>andreasschnitze</dc:creator>
      <dc:date>2017-07-06T15:13:39Z</dc:date>
    </item>
  </channel>
</rss>