<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC824 CLOCKOUT CMSIS PINASSIGN11 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-CLOCKOUT-CMSIS-PINASSIGN11/m-p/566735#M17382</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by besterm on Tue Jul 14 07:35:01 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I had the same issue and after looking at the datasheet, decided to modify my header file to include the missing pinassign entries (9-11).&amp;nbsp; I was then able to assign the clkout pin function to an IO pin and it works fine now.&amp;nbsp; Just remember if you add these entries, to also change the PINASSIGN array from 9 to 12 and to change the RESERVED0 array from 103 to 100 to account for the 3 new pinassign entries.&amp;nbsp; &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 20:06:13 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T20:06:13Z</dc:date>
    <item>
      <title>LPC824 CLOCKOUT CMSIS PINASSIGN11</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-CLOCKOUT-CMSIS-PINASSIGN11/m-p/566733#M17380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by kiryat8 on Tue May 05 01:03:04 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the latest CMSIS definitions "CMSIS 3.20 March 2013 release."&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;There is no&amp;nbsp; PINASSIGN11 definition in LPC8xx.h for routing the CLKOUT function as written in the pdf.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I see in the LPC open project there are&amp;nbsp; PINASSIGN11 definitions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;SWM_ADC_PINTRIG1_I = 0xB0,&amp;nbsp;&amp;nbsp; /*!&amp;lt; PINASSIGN11 - ADC PIN TRIGGER-1 Input */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SWM_ACMP_O_O,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; PINASSIGN11 - ACMP OUT Output */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SWM_CLKOUT_O,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; PINASSIGN11 - CLKOUT Output */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SWM_GPIO_INT_BMAT_O,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; PINASSIGN11 - GPIO INT BMAT Output */&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does the LPC824 have the ability to route its clock out?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can I add PINASSIGN11 definitions to the header file?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; David Kaplan&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:06:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-CLOCKOUT-CMSIS-PINASSIGN11/m-p/566733#M17380</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:06:11Z</dc:date>
    </item>
    <item>
      <title>Re: LPC824 CLOCKOUT CMSIS PINASSIGN11</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-CLOCKOUT-CMSIS-PINASSIGN11/m-p/566734#M17381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by embd02161991 on Tue May 05 15:13:37 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPC82x features a clock output function that routes the IRC, the SysOsc, the watchdog oscillator, or the main clock to the CLKOUT function. The CLKOUT function can be connected to any digital pin through the switch matrix.You can use the PINASSIGN11 definition for CLKOUT function assignment.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP Technical Support &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:06:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-CLOCKOUT-CMSIS-PINASSIGN11/m-p/566734#M17381</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:06:12Z</dc:date>
    </item>
    <item>
      <title>Re: LPC824 CLOCKOUT CMSIS PINASSIGN11</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-CLOCKOUT-CMSIS-PINASSIGN11/m-p/566735#M17382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by besterm on Tue Jul 14 07:35:01 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I had the same issue and after looking at the datasheet, decided to modify my header file to include the missing pinassign entries (9-11).&amp;nbsp; I was then able to assign the clkout pin function to an IO pin and it works fine now.&amp;nbsp; Just remember if you add these entries, to also change the PINASSIGN array from 9 to 12 and to change the RESERVED0 array from 103 to 100 to account for the 3 new pinassign entries.&amp;nbsp; &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:06:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-CLOCKOUT-CMSIS-PINASSIGN11/m-p/566735#M17382</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:06:13Z</dc:date>
    </item>
  </channel>
</rss>