<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1788 GPDMA Transfer size</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-GPDMA-Transfer-size/m-p/516539#M1733</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wella-tabor on Thu May 09 06:05:49 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Ok, I should read it :)&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;[from the ARM site]&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Scenario (1)&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;In the case where the DMAC is the flow controller, if I set Burst size (same for both source and destination) to 128 and width is word, then, should I set TransferSize to 512 i.e. 128*4, bytes or 128 (items of burst)? &lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Answer (1) The TransferSize is the number of transfers to perform when the DMAC is the flow controller. So, in your example, the TransferSize is 128; the total number of bytes transferred will be 128 x 4 = 512&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:21:43 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:21:43Z</dc:date>
    <item>
      <title>LPC1788 GPDMA Transfer size</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-GPDMA-Transfer-size/m-p/516538#M1732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wella-tabor on Thu May 09 05:53:59 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;does anybody know what is the meaning of the (bits)11:0 TRANSFERSIZE field in the DMA Channel Control registers? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Should it be number of transfers with a width DWIDTH =&amp;gt; number of transfered bytes = (2^DWIDTH) * TRANSFERSIZE?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It is not clear for me from the user manual v2.1. From PDL's DMA example it seems to be number of transfers, not bytes. I did not read ARM PL081 and I am trying to avoid this...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you for any hints&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Martin&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:21:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-GPDMA-Transfer-size/m-p/516538#M1732</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:21:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1788 GPDMA Transfer size</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-GPDMA-Transfer-size/m-p/516539#M1733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wella-tabor on Thu May 09 06:05:49 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Ok, I should read it :)&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;[from the ARM site]&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Scenario (1)&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;In the case where the DMAC is the flow controller, if I set Burst size (same for both source and destination) to 128 and width is word, then, should I set TransferSize to 512 i.e. 128*4, bytes or 128 (items of burst)? &lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Answer (1) The TransferSize is the number of transfers to perform when the DMAC is the flow controller. So, in your example, the TransferSize is 128; the total number of bytes transferred will be 128 x 4 = 512&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:21:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-GPDMA-Transfer-size/m-p/516539#M1733</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:21:43Z</dc:date>
    </item>
  </channel>
</rss>