<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Debugging M0 via openocd/gdb?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Debugging-M0-via-openocd-gdb/m-p/566245#M17263</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by omegahacker on Sun Jun 15 18:17:30 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm getting closer and closer to having FreeRTOS running properly on the M0, but I keep finding that it's going to be a lot faster if I can actually single-step what's going on.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have openocd 0.6.0 going with it's stock config files (include &amp;lt;adapter&amp;gt;, include &amp;lt;lpc4350&amp;gt;) and that works fine for the M4, but I have no idea how to actually attach GDB to the M0 without halting the M4 or anything else.&amp;nbsp; It'd be ideal if I could connect to it after my loader has set up the codebase, then reset the M0 via RGU registers and catch it during "boot".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any hints?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:51:35 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:51:35Z</dc:date>
    <item>
      <title>Debugging M0 via openocd/gdb?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Debugging-M0-via-openocd-gdb/m-p/566245#M17263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by omegahacker on Sun Jun 15 18:17:30 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm getting closer and closer to having FreeRTOS running properly on the M0, but I keep finding that it's going to be a lot faster if I can actually single-step what's going on.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have openocd 0.6.0 going with it's stock config files (include &amp;lt;adapter&amp;gt;, include &amp;lt;lpc4350&amp;gt;) and that works fine for the M4, but I have no idea how to actually attach GDB to the M0 without halting the M4 or anything else.&amp;nbsp; It'd be ideal if I could connect to it after my loader has set up the codebase, then reset the M0 via RGU registers and catch it during "boot".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any hints?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:51:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Debugging-M0-via-openocd-gdb/m-p/566245#M17263</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:51:35Z</dc:date>
    </item>
  </channel>
</rss>