<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Application ends up in NMI handler in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Application-ends-up-in-NMI-handler/m-p/566079#M17229</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by alston_gama on Thu Oct 30 06:53:40 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using LPC4357 controller development kit from Embedded Artist.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;we have a secondary boot loader (SBL) to load an application's binary file from SD card to SDRAM and to execute from SDRAM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am able to execute Embedded Artist's sample code by using SBL properly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now i have integrated emWin graphics library to this project which partially works and causes NMI (Non Maskable Interrupt), that it ends up in NMI handler.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This is specifically found to cause due to 'Create Dialogue' function usage from emWin. (where as it works perfectly fine while executed from internal flash).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note: If i do not use above function and keep updating the GUI for cursor movement based on touch, it works just fine!!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any pointer with this regard would be highly appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:49:34 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:49:34Z</dc:date>
    <item>
      <title>Application ends up in NMI handler</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Application-ends-up-in-NMI-handler/m-p/566079#M17229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by alston_gama on Thu Oct 30 06:53:40 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using LPC4357 controller development kit from Embedded Artist.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;we have a secondary boot loader (SBL) to load an application's binary file from SD card to SDRAM and to execute from SDRAM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am able to execute Embedded Artist's sample code by using SBL properly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now i have integrated emWin graphics library to this project which partially works and causes NMI (Non Maskable Interrupt), that it ends up in NMI handler.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This is specifically found to cause due to 'Create Dialogue' function usage from emWin. (where as it works perfectly fine while executed from internal flash).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note: If i do not use above function and keep updating the GUI for cursor movement based on touch, it works just fine!!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any pointer with this regard would be highly appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:49:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Application-ends-up-in-NMI-handler/m-p/566079#M17229</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:49:34Z</dc:date>
    </item>
    <item>
      <title>Re: Application ends up in NMI handler</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Application-ends-up-in-NMI-handler/m-p/566080#M17230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I'm having a very similar issue currently with the NXP LPC1857.&amp;nbsp; Were you ever able to figure out what was causing the application to enter the NMI Handler?&amp;nbsp; Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jun 2018 23:06:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Application-ends-up-in-NMI-handler/m-p/566080#M17230</guid>
      <dc:creator>jamestasker</dc:creator>
      <dc:date>2018-06-14T23:06:32Z</dc:date>
    </item>
  </channel>
</rss>