<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: DMA transfer from register PIN0 or MPIN0 to RAM on 824 chip</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/DMA-transfer-from-register-PIN0-or-MPIN0-to-RAM-on-824-chip/m-p/564881#M16973</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 19 Jun 2016 01:10:14 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-19T01:10:14Z</dc:date>
    <item>
      <title>DMA transfer from register PIN0 or MPIN0 to RAM on 824 chip</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DMA-transfer-from-register-PIN0-or-MPIN0-to-RAM-on-824-chip/m-p/564880#M16972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ntil on Sun May 08 04:42:05 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Good day all.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can DMA make transfers from PIN0 or MPIN0 registers to SRAM on 824 chip ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When I try it, i got DMA error. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Other memory-to-memory or UART-to-memory transfers works fine..&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It looks like not allowed to transfer with DMA from any register? only specific (SPI,UART, etc)..&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;but "LPC82x User manual" tells "The source and destination end addresses, as well as the link to the next descriptor are&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;just memory addresses that can point to any valid address on the device."&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So can I read with DMA any register or only specific?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:04:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DMA-transfer-from-register-PIN0-or-MPIN0-to-RAM-on-824-chip/m-p/564880#M16972</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:04:57Z</dc:date>
    </item>
    <item>
      <title>Re: DMA transfer from register PIN0 or MPIN0 to RAM on 824 chip</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DMA-transfer-from-register-PIN0-or-MPIN0-to-RAM-on-824-chip/m-p/564881#M16973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jun 2016 01:10:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DMA-transfer-from-register-PIN0-or-MPIN0-to-RAM-on-824-chip/m-p/564881#M16973</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-19T01:10:14Z</dc:date>
    </item>
  </channel>
</rss>