<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC810 Question about connect ACMP_O to SCT input in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC810-Question-about-connect-ACMP-O-to-SCT-input/m-p/564800#M16952</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by onkel.jack@t-online.de on Wed Jun 26 05:38:20 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;&amp;lt;span class="postbody"&amp;gt;User manual states: &lt;BR /&gt;You can use the comparator output function (ACMP_O) to start or stop the SCT or, more &lt;BR /&gt;generally, create an SCT event. To create an SCT event, connect AMP_O as follows: &lt;BR /&gt;1. Using the switch matrix, connect ACMP_O to a pin. See Table 203. &lt;BR /&gt;2. Using the switch matrix, connect any of the SCT input functions to the same pin. &lt;BR /&gt;See Table 107. &lt;BR /&gt;The selected SCT input can now monitor the ACMP_O function. &lt;BR /&gt;&lt;BR /&gt;My question now is: do i have to use a real exsiting pin or it is possible to use i.e. P0.6 which is physical not connected to a external pin ?&lt;BR /&gt;&amp;lt;/span&amp;gt;&amp;lt;span class="postbody"&amp;gt;This would save a physical pin carry a signal i dont need to connect outside of the MCU.&amp;lt;/span&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 20:04:52 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T20:04:52Z</dc:date>
    <item>
      <title>LPC810 Question about connect ACMP_O to SCT input</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC810-Question-about-connect-ACMP-O-to-SCT-input/m-p/564800#M16952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by onkel.jack@t-online.de on Wed Jun 26 05:38:20 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;&amp;lt;span class="postbody"&amp;gt;User manual states: &lt;BR /&gt;You can use the comparator output function (ACMP_O) to start or stop the SCT or, more &lt;BR /&gt;generally, create an SCT event. To create an SCT event, connect AMP_O as follows: &lt;BR /&gt;1. Using the switch matrix, connect ACMP_O to a pin. See Table 203. &lt;BR /&gt;2. Using the switch matrix, connect any of the SCT input functions to the same pin. &lt;BR /&gt;See Table 107. &lt;BR /&gt;The selected SCT input can now monitor the ACMP_O function. &lt;BR /&gt;&lt;BR /&gt;My question now is: do i have to use a real exsiting pin or it is possible to use i.e. P0.6 which is physical not connected to a external pin ?&lt;BR /&gt;&amp;lt;/span&amp;gt;&amp;lt;span class="postbody"&amp;gt;This would save a physical pin carry a signal i dont need to connect outside of the MCU.&amp;lt;/span&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:04:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC810-Question-about-connect-ACMP-O-to-SCT-input/m-p/564800#M16952</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:04:52Z</dc:date>
    </item>
    <item>
      <title>Re: LPC810 Question about connect ACMP_O to SCT input</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC810-Question-about-connect-ACMP-O-to-SCT-input/m-p/564801#M16953</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by NXP_Paul on Wed Aug 14 14:27:59 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;It is never a good idea to use a pin that does not exist in the device data sheet.&amp;nbsp; Although it may work in some situations, there is no guarantee that it will continue to function correctly in future device revisions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:04:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC810-Question-about-connect-ACMP-O-to-SCT-input/m-p/564801#M16953</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:04:53Z</dc:date>
    </item>
  </channel>
</rss>