<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLcd's Green4 can not be used with internal Rtc</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lcd-s-Green4-can-not-be-used-with-internal-Rtc/m-p/562990#M16587</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by askar on Thu Feb 05 06:00:58 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have been faced with a strange matter that need some help,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i am using a system that uses Lpc4357 with 208 pin LQFP package,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the processor pin number 181 is used as PB_5 and set to LCDVD14&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;that is used as bit4 for Green color&amp;nbsp; in LCD defined as RGB 5:6:5.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the pin number 182 is RTCX1 crystal signal used for internal Rtc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When i use the bit4 of Green color as described above, Rtc goes forward or backward for&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;example, 50 minutes every day, when I use PB_5 as a normal Gpio, then&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the Rtc operates accurately.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any Help is appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:48:55 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:48:55Z</dc:date>
    <item>
      <title>Lcd's Green4 can not be used with internal Rtc</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lcd-s-Green4-can-not-be-used-with-internal-Rtc/m-p/562990#M16587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by askar on Thu Feb 05 06:00:58 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have been faced with a strange matter that need some help,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i am using a system that uses Lpc4357 with 208 pin LQFP package,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the processor pin number 181 is used as PB_5 and set to LCDVD14&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;that is used as bit4 for Green color&amp;nbsp; in LCD defined as RGB 5:6:5.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the pin number 182 is RTCX1 crystal signal used for internal Rtc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When i use the bit4 of Green color as described above, Rtc goes forward or backward for&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;example, 50 minutes every day, when I use PB_5 as a normal Gpio, then&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the Rtc operates accurately.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any Help is appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:48:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Lcd-s-Green4-can-not-be-used-with-internal-Rtc/m-p/562990#M16587</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:48:55Z</dc:date>
    </item>
  </channel>
</rss>