<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC Link 2 is not working</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-is-not-working/m-p/562265#M16459</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Fri Nov 01 13:02:18 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;With your LPC800-MAX unpowered, press and hold down the Reset button.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now power the LPC800-MAX board up, whilst still holding the Reset button down.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now release the Reset button.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You should now be able to successfully start a debug session from LPCXpresso and connect to the LPC800-MAX board via your LPC-Link2.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso Support.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 20:03:00 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T20:03:00Z</dc:date>
    <item>
      <title>LPC Link 2 is not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-is-not-working/m-p/562262#M16456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Marqueses on Fri Nov 01 08:37:11 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have try to use my LPC Link 2 in CMSIS-DAP configuration to program LPC-800 board and LPC-812 board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I haven't success to program any of them with LPC Link 2, but yes with internal CMSIS-DAP onboard in LPC-812 board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The result is this:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ni: LPCXpresso RedlinkMulti Driver v6.0 (Sep 17 2013 18:02:04 - crt_emu_cm_redlink.exe build 244)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Pc: (&amp;nbsp; 0) Reading remote configuration&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Nc: Looked for chip XML file in C:/nxp/LPCXpresso_6.1.0_164/lpcxpresso/bin/LPC812.xml&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Nc: Looked for vendor directory XML file in C:/nxp/LPCXpresso_6.1.0_164/lpcxpresso/bin/NXP_directory.xml&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Nc: Found generic directory XML file in C:/nxp/LPCXpresso_6.1.0_164/lpcxpresso/bin/crt_directory.xml&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Pc: (&amp;nbsp; 5) Remote configuration complete&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ed:02: Failed on connect: Ee(36). Could not connect to core.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Et: Emu(0): Conn&amp;amp;Reset. Was: None. DpID: 00000000. CpuID: 00000000. Info: (null)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Error 0: (null)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Last sticky: 0. AIndex: 0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;No MemAp selected&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Pc: (100) Target Connection Failed&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could anyone tell if have used LPC Link 2 and if it works? Is this programmer only able to program nxp µC?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:02:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-is-not-working/m-p/562262#M16456</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:02:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPC Link 2 is not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-is-not-working/m-p/562263#M16457</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Fri Nov 01 09:29:55 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I've just used LPC-Link2 programmed with the latest CMSIS-DAP firmware (v1.11) to debug an LPC800-MAX board from LPCXpresso v6.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The one gotcha if you are using an LPC800-MAX, which I suspect you might be hitting, is that in order to debug this board with an external debug probe, you need to power up the board with SW1 (Reset) depressed - in order to prevent the onboard debug probe taking control of the LPC812.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If this doesn't get you going, please post more details of the boards that you are trying to connect to.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso Support&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:02:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-is-not-working/m-p/562263#M16457</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:02:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPC Link 2 is not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-is-not-working/m-p/562264#M16458</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Marqueses on Fri Nov 01 10:38:10 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I don't understand you very well what do you want me to do with Reset button in target board. Anyway, I have tried to download the release code with and without pressing it and it still fail.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have some pics maybe it could help you to give me a clue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Some others points...I have v1.10 of CMSIS-DAP too. With the CMSIS-DAP from LPCMAX-800 is working perfect. LPCMAX-800 is supplied by LPC Link 2 (also tested separated by two usb cables from PC).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I don't what more information could be useful. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards. &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:02:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-is-not-working/m-p/562264#M16458</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:02:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPC Link 2 is not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-is-not-working/m-p/562265#M16459</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Fri Nov 01 13:02:18 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;With your LPC800-MAX unpowered, press and hold down the Reset button.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now power the LPC800-MAX board up, whilst still holding the Reset button down.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now release the Reset button.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You should now be able to successfully start a debug session from LPCXpresso and connect to the LPC800-MAX board via your LPC-Link2.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso Support.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:03:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-is-not-working/m-p/562265#M16459</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:03:00Z</dc:date>
    </item>
  </channel>
</rss>