<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC1115 debugging works, but not flashing in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1115-debugging-works-but-not-flashing/m-p/561784#M16349</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have&amp;nbsp; custom board with an lpc1115. It is working fine debugging over TWI.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, when I try to flash the .axf file I have built onto the board, it proceeds with the flashing OK, but the unit does not send anything out of the uart (which is does when I debug over TWI).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas as to what could cause this? I have modified the memory details of the chip to reserve the upper part of flash for saving configuration. ie. the size of MFlash64 is set to 0x9000 and not 0x10000&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Jun 2016 11:23:58 GMT</pubDate>
    <dc:creator>nfogh</dc:creator>
    <dc:date>2016-06-22T11:23:58Z</dc:date>
    <item>
      <title>LPC1115 debugging works, but not flashing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1115-debugging-works-but-not-flashing/m-p/561784#M16349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have&amp;nbsp; custom board with an lpc1115. It is working fine debugging over TWI.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, when I try to flash the .axf file I have built onto the board, it proceeds with the flashing OK, but the unit does not send anything out of the uart (which is does when I debug over TWI).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas as to what could cause this? I have modified the memory details of the chip to reserve the upper part of flash for saving configuration. ie. the size of MFlash64 is set to 0x9000 and not 0x10000&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jun 2016 11:23:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1115-debugging-works-but-not-flashing/m-p/561784#M16349</guid>
      <dc:creator>nfogh</dc:creator>
      <dc:date>2016-06-22T11:23:58Z</dc:date>
    </item>
  </channel>
</rss>