<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 lpc4330 MII Interface TFBGA180, pin missing?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc4330-MII-Interface-TFBGA180-pin-missing/m-p/561217#M16244</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ljminti on Thu Mar 31 06:17:04 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;during reading the LPC43xx Datasheet, i'm a little confused about the MII Interface.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If i'm right, the LPC4330FET180 has an MII-Interface. However the ENET_RX_CLK as well as the ENET_TX_ER Signal that is used for the external PHY is only avalable in the BGA256 package.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The question is now, how to connect the BGA180 version with MII-Interface to an external PHY?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Julien&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:46:01 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:46:01Z</dc:date>
    <item>
      <title>lpc4330 MII Interface TFBGA180, pin missing?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc4330-MII-Interface-TFBGA180-pin-missing/m-p/561217#M16244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ljminti on Thu Mar 31 06:17:04 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;during reading the LPC43xx Datasheet, i'm a little confused about the MII Interface.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If i'm right, the LPC4330FET180 has an MII-Interface. However the ENET_RX_CLK as well as the ENET_TX_ER Signal that is used for the external PHY is only avalable in the BGA256 package.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The question is now, how to connect the BGA180 version with MII-Interface to an external PHY?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Julien&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:46:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc4330-MII-Interface-TFBGA180-pin-missing/m-p/561217#M16244</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:46:01Z</dc:date>
    </item>
    <item>
      <title>Re: lpc4330 MII Interface TFBGA180, pin missing?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc4330-MII-Interface-TFBGA180-pin-missing/m-p/561218#M16245</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Thu Mar 31 20:23:10 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Perhaps you have to use RMII on that package.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Mike.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:46:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc4330-MII-Interface-TFBGA180-pin-missing/m-p/561218#M16245</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:46:02Z</dc:date>
    </item>
    <item>
      <title>Re: lpc4330 MII Interface TFBGA180, pin missing?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc4330-MII-Interface-TFBGA180-pin-missing/m-p/561219#M16246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ljminti on Thu Mar 31 23:55:40 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Well, &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;in the Datasheet (page 819) it is written:&lt;/SPAN&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;The MII is not available on the LQFP144 and TFBGA100 packages.&lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For me the package TFBGA180 is ready for MII.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:46:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc4330-MII-Interface-TFBGA180-pin-missing/m-p/561219#M16246</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:46:03Z</dc:date>
    </item>
    <item>
      <title>Re: lpc4330 MII Interface TFBGA180, pin missing?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc4330-MII-Interface-TFBGA180-pin-missing/m-p/561220#M16247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jun 2016 01:06:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc4330-MII-Interface-TFBGA180-pin-missing/m-p/561220#M16247</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-19T01:06:45Z</dc:date>
    </item>
  </channel>
</rss>