<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC824 Drivers for the Adafruit Motor Shield (v2)</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-Drivers-for-the-Adafruit-Motor-Shield-v2/m-p/560950#M16185</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ktownsend on Thu Oct 02 03:46:31 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I was able to get my hands on an early sample of the LPC82x LPCXpresso board, and put together some drivers for Adafruit's Motor Shield (v2) to test the MCU out.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've been really impressed with the LPC82x as an upgrade from the LPC81x series, and the Arduino style headers make it relatively easy to gain access to a lot of existing HW.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;If you're interested in trying the Arduino-style headers out with a readily available shield I've published the motor shield drivers on Github here: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fgithub.com%2Fmicrobuilder%2FLPC824_MotorShieldv2_Drivers" rel="nofollow" target="_blank"&gt;https://github.com/microbuilder/LPC824_MotorShieldv2_Drivers&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The drivers make use of the ROM-based I2C drivers (in polling mode), and the SCTimer to driver either DC or servo motors.&amp;nbsp; The LPCOpen library is also used, and will need to be downloaded and the following libraries must exist in the same workspace: &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*] lpc_chip_82x&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*] lpc_board_nxp_lpcxpresso_824&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I hope this is of help to someone!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:59:54 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:59:54Z</dc:date>
    <item>
      <title>LPC824 Drivers for the Adafruit Motor Shield (v2)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-Drivers-for-the-Adafruit-Motor-Shield-v2/m-p/560950#M16185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ktownsend on Thu Oct 02 03:46:31 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I was able to get my hands on an early sample of the LPC82x LPCXpresso board, and put together some drivers for Adafruit's Motor Shield (v2) to test the MCU out.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've been really impressed with the LPC82x as an upgrade from the LPC81x series, and the Arduino style headers make it relatively easy to gain access to a lot of existing HW.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;If you're interested in trying the Arduino-style headers out with a readily available shield I've published the motor shield drivers on Github here: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fgithub.com%2Fmicrobuilder%2FLPC824_MotorShieldv2_Drivers" rel="nofollow" target="_blank"&gt;https://github.com/microbuilder/LPC824_MotorShieldv2_Drivers&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The drivers make use of the ROM-based I2C drivers (in polling mode), and the SCTimer to driver either DC or servo motors.&amp;nbsp; The LPCOpen library is also used, and will need to be downloaded and the following libraries must exist in the same workspace: &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*] lpc_chip_82x&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*] lpc_board_nxp_lpcxpresso_824&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I hope this is of help to someone!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:59:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-Drivers-for-the-Adafruit-Motor-Shield-v2/m-p/560950#M16185</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:59:54Z</dc:date>
    </item>
  </channel>
</rss>