<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Flash Magic cannnot connect to LPC810</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-Magic-cannnot-connect-to-LPC810/m-p/560713#M16147</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by changchao on Mon Mar 21 19:02:51 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have two LPC810s,under the same wiring(see the image below),&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;One can be connected by Flash Magic,and the other one cannot be ( "the Operation Failed.(failed to autobaud - Step1) message" showed when ISP -&amp;gt; Read Security).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So my question is,is there a way to tell the reason is that some pins are just switched off by Switch Matrix Tool(maybe I did before) or the MCU was damaged.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried to Boot the failed one into ISP mode following the "Regaining debug access to target MCU" FAQ,but wihout a success.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;May be I'm not understanding the procedure correctly,the one I followed is&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;gt;The procedure is then to GND the ISP pin, assert RST, then remove the GND to ISP pin. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1.GND the ISP pin(pin 5)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2.GND the RST pin(pin 1)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3.power on&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4.pull the Jumper wire of ISP PIN&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2016/03/23 updated:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Also,I cannot debug the damaged(?) LPC810 using LPCXpresso IDE,while the other LPC810 works well.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can it be that the CRP mode is set so that I can neither go into ISP mode nor connect by Flash Magic,If this is the case,Is there a way to recover from it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:59:20 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:59:20Z</dc:date>
    <item>
      <title>Flash Magic cannnot connect to LPC810</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-Magic-cannnot-connect-to-LPC810/m-p/560713#M16147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by changchao on Mon Mar 21 19:02:51 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have two LPC810s,under the same wiring(see the image below),&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;One can be connected by Flash Magic,and the other one cannot be ( "the Operation Failed.(failed to autobaud - Step1) message" showed when ISP -&amp;gt; Read Security).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So my question is,is there a way to tell the reason is that some pins are just switched off by Switch Matrix Tool(maybe I did before) or the MCU was damaged.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried to Boot the failed one into ISP mode following the "Regaining debug access to target MCU" FAQ,but wihout a success.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;May be I'm not understanding the procedure correctly,the one I followed is&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;gt;The procedure is then to GND the ISP pin, assert RST, then remove the GND to ISP pin. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1.GND the ISP pin(pin 5)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2.GND the RST pin(pin 1)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3.power on&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4.pull the Jumper wire of ISP PIN&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2016/03/23 updated:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Also,I cannot debug the damaged(?) LPC810 using LPCXpresso IDE,while the other LPC810 works well.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can it be that the CRP mode is set so that I can neither go into ISP mode nor connect by Flash Magic,If this is the case,Is there a way to recover from it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:59:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-Magic-cannnot-connect-to-LPC810/m-p/560713#M16147</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:59:20Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Magic cannnot connect to LPC810</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-Magic-cannnot-connect-to-LPC810/m-p/560714#M16148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jun 2016 01:05:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-Magic-cannnot-connect-to-LPC810/m-p/560714#M16148</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-19T01:05:59Z</dc:date>
    </item>
  </channel>
</rss>