<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC4337 has crashed in debug mode and flash programming isn't working since then in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-has-crashed-in-debug-mode-and-flash-programming-isn-t/m-p/560318#M16060</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jgorsk on Fri Oct 05 07:02:15 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I changed the state of the boot config pins and then I was able &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;to program the chip via JTAG. It works fine now.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:43:48 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:43:48Z</dc:date>
    <item>
      <title>LPC4337 has crashed in debug mode and flash programming isn't working since then</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-has-crashed-in-debug-mode-and-flash-programming-isn-t/m-p/560315#M16057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jgorsk on Tue Oct 02 09:53:12 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC4337 has crashed in debug mode. It's not possible to use the chip since then. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;JTAG interface seems to be working but flash programming or erasing over JTAG isn't. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I get this message in Keil when I try to erase the flash memory&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;'Cannot Load Flash Programming Algorithm'.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I start the debugger there is an additional message in the output window&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Cannot Write to RAM for Flash Algorithms !&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Erase Failed!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there a solution to this problem or should I replace that chip?&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:43:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-has-crashed-in-debug-mode-and-flash-programming-isn-t/m-p/560315#M16057</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:43:46Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4337 has crashed in debug mode and flash programming isn't working since then</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-has-crashed-in-debug-mode-and-flash-programming-isn-t/m-p/560316#M16058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by fcarlo on Tue Oct 02 23:42:15 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;You should be able to recover the uC putting it in ISP programming mode (you can use DFU, for example).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fproject%2Fdfu-download-programming-utility-and-security-lpcdfusec-tool" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/project/dfu-download-programming-utility-and-security-lpcdfusec-tool&lt;/A&gt;&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:43:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-has-crashed-in-debug-mode-and-flash-programming-isn-t/m-p/560316#M16058</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:43:47Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4337 has crashed in debug mode and flash programming isn't working since then</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-has-crashed-in-debug-mode-and-flash-programming-isn-t/m-p/560317#M16059</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bavarian on Thu Oct 04 04:23:56 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;If there is still access via JTAG/SWD, then it should be possible to recover, As I can see different reasons for this problem, here are different hints how to overcome it:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1) Play with the settings for the reset: &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Project Settings --&amp;gt; Debug --&amp;gt; Settings&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; - Autodetect&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; - VECTRESET&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2) Power-on your board in a different bootmode configuration, (e.g. the UART or USB bootmode) before you try programming. This ensures that the chip does not run into a software in the flash which maybe causes this lockout.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;3) Use the DFU utility (USB bootmode) to program the flash.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;4) Use the latest version of FlashMagic to get flash programming access over UART. (overall a little bit more complicated than the other proposals).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP Technical Support Team&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:43:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-has-crashed-in-debug-mode-and-flash-programming-isn-t/m-p/560317#M16059</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:43:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4337 has crashed in debug mode and flash programming isn't working since then</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-has-crashed-in-debug-mode-and-flash-programming-isn-t/m-p/560318#M16060</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jgorsk on Fri Oct 05 07:02:15 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I changed the state of the boot config pins and then I was able &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;to program the chip via JTAG. It works fine now.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:43:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-has-crashed-in-debug-mode-and-flash-programming-isn-t/m-p/560318#M16060</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:43:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4337 has crashed in debug mode and flash programming isn't working since then</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-has-crashed-in-debug-mode-and-flash-programming-isn-t/m-p/560319#M16061</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by PhilYoung on Sat Oct 20 15:57:11 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;this is a common error message when the flash programming algorithms are not configured correctly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I noticed that the latest config for the LPC43xx seems to specify a ram size of 0x800 which is too small, increasing this to 0x8000 seems to work. This was for external flash programming but may be the same problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:43:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-has-crashed-in-debug-mode-and-flash-programming-isn-t/m-p/560319#M16061</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:43:49Z</dc:date>
    </item>
  </channel>
</rss>