<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC812 SCTimer in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559785#M15944</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by trimarco232 on Tue Apr 28 14:21:20 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;So my vias under LQFPs are illegal&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt; :bigsmile:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;writing : " tracks trough pass &lt;/SPAN&gt;&lt;STRONG&gt;and&lt;/STRONG&gt;&lt;SPAN&gt; vias under the chip" I though "both of then"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;Nice harangue&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;not only : an nxp's college has big succes with an TSSOP20 chip. But it has no analog comparator and I need one. &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 20:03:06 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T20:03:06Z</dc:date>
    <item>
      <title>LPC812 SCTimer</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559779#M15938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by trimarco232 on Tue Apr 28 04:55:55 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am interested for LPC812M101FDH16 because it has sexy size and incorporates an analogic comparator.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But before beginning in the LPC world (and of course with the SCTimer), I want to tell some question, here about the SCTimer :&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It supports:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– 4 inputs&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– 4 outputs&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– 5 match/capture registers&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– 6 events&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;– 2 states&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This what I need :&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 3 pwm outputs at ~20 kHz ;&amp;nbsp; 8bits are enough for the&amp;nbsp; resolution of the duty cycle ; two of these ouputs control the drivers of an 1/2 bridge&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 1 square wawe generator 1 ~ 2 kHz,&amp;nbsp; resolution = 1µs&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 1 capture, 16 bits wide and 1/2 µs resolution&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The way I have created that for other brand controller :&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1 timer is configured as 8bits pwm with 3 outputs&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1 othe timer that runs 16 bits up. The square output is made by an output toggle on compare match. An interruption is generated in order to update the compare register. The compare is trigered by an external source. An interruption is genrated in order to read and store the capture register.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The capture must be triggered by the output of the inside comparator, and have a digital filter.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please, tell me just if this is possible, thank you. (If yes, I will probably post for further explanation in the future)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:03:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559779#M15938</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:03:01Z</dc:date>
    </item>
    <item>
      <title>Re: LPC812 SCTimer</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559780#M15939</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by starblue on Tue Apr 28 06:30:39 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;My guess is that you will run out of match/capture registers: 4 match registers for the PWM, 1 match register for the square wave and 1 capture register is one too many. &lt;/SPAN&gt;&lt;STRONG&gt;Edit:&lt;/STRONG&gt;&lt;SPAN&gt; Maybe it is possible to do it because the registers are split into two 16-bit halves, but it is not clear to me.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You could take a look at the LPC82x, it has a bigger SCT, is also available in small packages and not much more expensive.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:03:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559780#M15939</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:03:03Z</dc:date>
    </item>
    <item>
      <title>Re: LPC812 SCTimer</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559781#M15940</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by trimarco232 on Tue Apr 28 11:20:59 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi starblue,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;thank you&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;well, I assume that the 4 compare match registers you refer to are the 3 pwm duty cycles and the 4th for the max of the the PWM ? Is there a way to avoid the 4th ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;the LPC82x, it has a bigger SCT&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;price is not an issue, but the 16TSSOP size is the best for my project, because I have no more room on my PCB, and my skills don't allow me to solder TQFP packages&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:03:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559781#M15940</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:03:03Z</dc:date>
    </item>
    <item>
      <title>Re: LPC812 SCTimer</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559782#M15941</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by R2D2 on Tue Apr 28 11:33:06 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: trimarco232&lt;/STRONG&gt;&lt;BR /&gt;...and my skills don't allow me to solder TQFP packages&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; :O&amp;nbsp; :((&amp;nbsp; :quest: &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Then it's time to learn it:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.youtube.com%2Fwatch%3Fv%3DTJAByNlfkyE" rel="nofollow" target="_blank"&gt;https://www.youtube.com/watch?v=TJAByNlfkyE&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:03:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559782#M15941</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:03:04Z</dc:date>
    </item>
    <item>
      <title>Re: LPC812 SCTimer</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559783#M15942</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by trimarco232 on Tue Apr 28 13:19:10 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;of course R2D2, thanks !&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;but SSOP packages have other advantages, like allowing tracks trough pass and vias under the chip&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and nxp says :&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;" these packages help to streamline prototyping, ease of assembly, and simplify high-volume, low-cost manufacturing. Further, the LPC800 TSSOP packages are designed for scalability by mapping power, ground and analog functions to identical locations so designers can move from TSSOP16 to TSSOP20 packages with minimal effort " &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:03:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559783#M15942</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:03:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPC812 SCTimer</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559784#M15943</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by R2D2 on Tue Apr 28 13:53:37 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: trimarco232&lt;/STRONG&gt;&lt;BR /&gt;but SSOP packages have other advantages, like allowing tracks trough pass and vias under the chip...&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; :O So my vias under LQFPs are illegal&amp;nbsp; :quest: &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: trimarco232&lt;/STRONG&gt;&lt;BR /&gt;nxp says :&lt;BR /&gt;" these packages help to streamline prototyping, ease of assembly, and simplify high-volume, low-cost manufacturing. Further, the LPC800 TSSOP packages are designed for scalability by mapping power, ground and analog functions to identical locations so designers can move from TSSOP16 to TSSOP20 packages with minimal effort "&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Nice harangue, unfortunately they don't manufacture a lot of chips in TSSOP&amp;nbsp; :(( &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;(Or did I overlook the LPC1549 TSSOP48&amp;nbsp; :D&amp;nbsp; )&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:03:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559784#M15943</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:03:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPC812 SCTimer</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559785#M15944</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by trimarco232 on Tue Apr 28 14:21:20 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;So my vias under LQFPs are illegal&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt; :bigsmile:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;writing : " tracks trough pass &lt;/SPAN&gt;&lt;STRONG&gt;and&lt;/STRONG&gt;&lt;SPAN&gt; vias under the chip" I though "both of then"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;Nice harangue&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;not only : an nxp's college has big succes with an TSSOP20 chip. But it has no analog comparator and I need one. &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:03:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559785#M15944</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:03:06Z</dc:date>
    </item>
    <item>
      <title>Re: LPC812 SCTimer</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559786#M15945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by starblue on Wed Apr 29 00:24:49 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: trimarco232&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;well, I assume that the 4 compare match registers you refer to are the 3 pwm duty cycles and the 4th for the max of the the PWM?&lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN&gt;Yes.&lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;Is there a way to avoid the 4th ?&lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN&gt;I don't think so, unless maybe when your period is exactly 2^16 clock cycles, which is not the case.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;the LPC82x, it has a bigger SCT&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;price is not an issue, but the 16TSSOP size is the best for my project, because I have no more room on my PCB, and my skills don't allow me to solder TQFP packages&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It is available as TSSOP20 and HVQFN33, not TQFP. HVQFN33 is about the same size as TSSOP16, but I would also consider it difficult to solder (I haven't tried QFN yet, TQFP is fine with me).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;TSSOP20 is just 1.3mm longer than TSSOP16, is it really that tight on your board?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:03:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559786#M15945</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:03:06Z</dc:date>
    </item>
    <item>
      <title>Re: LPC812 SCTimer</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559787#M15946</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by trimarco232 on Wed Apr 29 03:07:05 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;TSSOP20 is just 1.3mm longer than TSSOP16&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;right !&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt; is it really that tight on your board?&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;you can see the attached drawings, I didn't design it yet, but an other version will be smaller (not so wide), and I want to use the same schematic for all versions&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt; &lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt; &lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Is there a way to avoid the 4th ?&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;I don't think so, unless maybe when your period is exactly 2^16 clock cycles, which is not the case.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You are probably right. So it might be a walk around : two of the pwm outputs drives a 1/2 bridge connected to a little dc motor. The upper transistor is to control the speed, the lower is to control&amp;nbsp; the brake. That means the pwms are never used at same time. Mi idea is to use the same pwm to drive once the upper, once the lower, just redirecting the pwm through the switch matrix ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:03:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC812-SCTimer/m-p/559787#M15946</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:03:07Z</dc:date>
    </item>
  </channel>
</rss>