<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックReading Serial Number of Flashless LPC43xx devices</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Reading-Serial-Number-of-Flashless-LPC43xx-devices/m-p/558371#M15589</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by twhittam on Fri Nov 29 09:46:58 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to be able to uniquely identify individual LPC4330 chips.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;On LPC43xx devices with onboard FLASH, command 58 of the IAP can be used to read the device serial number. Is there a way I can read this serial number on a Flashless part?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I know from &lt;/SPAN&gt;&lt;A href="http://http://www.lpcware.com/content/forum/lpcopen-v103-otp-programming-lpc4350"&gt;another post&lt;/A&gt;&lt;SPAN&gt; that addresses 0x40045000 and 0x40045000C hold values that will identify the device type. I can also see that address 0x40045004 holds a 32-bit value that seems to remain constant through a power cycle but is different from unit to unit.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could it be that the 4 words returned by IAP command 58 are the 4, 32-bit values starting at address 0x40045000?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your help.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Tony&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:43:26 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:43:26Z</dc:date>
    <item>
      <title>Reading Serial Number of Flashless LPC43xx devices</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Reading-Serial-Number-of-Flashless-LPC43xx-devices/m-p/558371#M15589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by twhittam on Fri Nov 29 09:46:58 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to be able to uniquely identify individual LPC4330 chips.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;On LPC43xx devices with onboard FLASH, command 58 of the IAP can be used to read the device serial number. Is there a way I can read this serial number on a Flashless part?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I know from &lt;/SPAN&gt;&lt;A href="http://http://www.lpcware.com/content/forum/lpcopen-v103-otp-programming-lpc4350"&gt;another post&lt;/A&gt;&lt;SPAN&gt; that addresses 0x40045000 and 0x40045000C hold values that will identify the device type. I can also see that address 0x40045004 holds a 32-bit value that seems to remain constant through a power cycle but is different from unit to unit.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could it be that the 4 words returned by IAP command 58 are the 4, 32-bit values starting at address 0x40045000?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your help.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Tony&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:43:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Reading-Serial-Number-of-Flashless-LPC43xx-devices/m-p/558371#M15589</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:43:26Z</dc:date>
    </item>
  </channel>
</rss>