<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Device is not rcognized when a Aardvark slave is connected to I2C2 pins</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Device-is-not-rcognized-when-a-Aardvark-slave-is-connected-to/m-p/558339#M15587</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jam on Sun May 03 22:36:51 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, Thanks for reply.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I could not understand what are you referring by software on the MCU!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried to put MCU in ISP mode by pressing SW2 while resetting the target but this does not help.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Jam&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:57:18 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:57:18Z</dc:date>
    <item>
      <title>Device is not rcognized when a Aardvark slave is connected to I2C2 pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Device-is-not-rcognized-when-a-Aardvark-slave-is-connected-to/m-p/558337#M15585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jam on Thu Apr 30 10:00:42 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am working with LPC54102 Xpresso V2 board. I am facing a problem that device is not recognized by J-link when I have connected a slave(Aardvark) with I2C2 pins.I see this message on J-link Commander &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"No device found on FINE interface.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Did not find any core.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;No device found at all. Selecting JTAG as default target interface."&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; When I disconnect the Aardvark then device is recognized. I see this message on J-link Commander &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"Info: TPIU fitted.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Info: ETM fitted.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Cortex-M4 identified.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Target interface speed: 100 kHz"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also in the above use case, In case of Xpresso IDE, I am able to load using red link server but auto execution from flash does not take place when I terminate the launch or reset the target.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I do not face this problem when Aardvark is connected to I2c0 or i2c1 pins.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It seems me problem with hardware, Can any help out?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Jam&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:57:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Device-is-not-rcognized-when-a-Aardvark-slave-is-connected-to/m-p/558337#M15585</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:57:16Z</dc:date>
    </item>
    <item>
      <title>Re: Device is not rcognized when a Aardvark slave is connected to I2C2 pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Device-is-not-rcognized-when-a-Aardvark-slave-is-connected-to/m-p/558338#M15586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nerd herd on Fri May 01 08:50:24 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi jam,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What software is on the MCU (irrespective of whether the Aardvark is connected to the LPC54102 or not)? If it is a hardware issue, you should be able to change the software and recreate the issue. Have you tried putting the MCU into ISP mode and connecting the Aardvark?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:57:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Device-is-not-rcognized-when-a-Aardvark-slave-is-connected-to/m-p/558338#M15586</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:57:17Z</dc:date>
    </item>
    <item>
      <title>Re: Device is not rcognized when a Aardvark slave is connected to I2C2 pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Device-is-not-rcognized-when-a-Aardvark-slave-is-connected-to/m-p/558339#M15587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jam on Sun May 03 22:36:51 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, Thanks for reply.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I could not understand what are you referring by software on the MCU!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried to put MCU in ISP mode by pressing SW2 while resetting the target but this does not help.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Jam&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:57:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Device-is-not-rcognized-when-a-Aardvark-slave-is-connected-to/m-p/558339#M15587</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:57:18Z</dc:date>
    </item>
    <item>
      <title>Re: Device is not rcognized when a Aardvark slave is connected to I2C2 pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Device-is-not-rcognized-when-a-Aardvark-slave-is-connected-to/m-p/558340#M15588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nerd herd on Wed May 06 08:34:16 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Jam,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Just for clarity, can you perform these steps to put the MCU into ISP mode and tell me what you see?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1) Unpower the board and disconnect the Aardvark.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2) Hold down the ISP pin (SW2) while plugging in power to the USB port (J4 if you are using an external J-Link).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3) Use J-Link Commander to see if it can detect the core. From your first post it sounds like you should be able to.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4) If the core was successfully detected, please repeat steps 1-3 with the exception of connecting the Aardvark in step one.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;After step 4, does J-Link Commander detect the core?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:57:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Device-is-not-rcognized-when-a-Aardvark-slave-is-connected-to/m-p/558340#M15588</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:57:19Z</dc:date>
    </item>
  </channel>
</rss>