<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックDual USB to Ethernet Converter using LPC1837</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-USB-to-Ethernet-Converter-using-LPC1837/m-p/556318#M15144</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need a dual USB to Ethernet converter solution. At one end I have a 3G Module and a WiFi Module, both have USB&amp;nbsp;interface ports. On the other end I have a Single Board Computer that has a Ethernet port. I want to know that if it is possible to connect both 3G and WiFi modules to Single Board Computer using the LPC1837 solution?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Hur Haider&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Aug 2016 12:44:00 GMT</pubDate>
    <dc:creator>hurhaider</dc:creator>
    <dc:date>2016-08-24T12:44:00Z</dc:date>
    <item>
      <title>Dual USB to Ethernet Converter using LPC1837</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-USB-to-Ethernet-Converter-using-LPC1837/m-p/556318#M15144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need a dual USB to Ethernet converter solution. At one end I have a 3G Module and a WiFi Module, both have USB&amp;nbsp;interface ports. On the other end I have a Single Board Computer that has a Ethernet port. I want to know that if it is possible to connect both 3G and WiFi modules to Single Board Computer using the LPC1837 solution?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Hur Haider&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 12:44:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-USB-to-Ethernet-Converter-using-LPC1837/m-p/556318#M15144</guid>
      <dc:creator>hurhaider</dc:creator>
      <dc:date>2016-08-24T12:44:00Z</dc:date>
    </item>
    <item>
      <title>Re: Dual USB to Ethernet Converter using LPC1837</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-USB-to-Ethernet-Converter-using-LPC1837/m-p/556319#M15145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it's possible. If you need two USB high speed ports, then you need to provide an external ULPI PHY for USB1, the integrated PHY can only do fully speed. USB and Ethernet have good DMA support, so if you need to achieve a good data throughput, then &amp;nbsp;the LPC1837 is a good choice.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;NXP Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Aug 2016 10:02:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-USB-to-Ethernet-Converter-using-LPC1837/m-p/556319#M15145</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2016-08-26T10:02:32Z</dc:date>
    </item>
    <item>
      <title>Re: Dual USB to Ethernet Converter using LPC1837</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-USB-to-Ethernet-Converter-using-LPC1837/m-p/556320#M15146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are there any schematics available for the LPC1837 Dual USB Host/Device Solution board ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Hur Haider&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2016 12:51:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-USB-to-Ethernet-Converter-using-LPC1837/m-p/556320#M15146</guid>
      <dc:creator>hurhaider</dc:creator>
      <dc:date>2016-08-29T12:51:52Z</dc:date>
    </item>
    <item>
      <title>Re: Dual USB to Ethernet Converter using LPC1837</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-USB-to-Ethernet-Converter-using-LPC1837/m-p/556321#M15147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Look out for application note AN11309. As the ISP1507 ULPI PHY from good old NXP times is no longer available, I recommend to go for one of the devices from the&amp;nbsp;Microchip USB33xx series.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;NXP Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2016 14:11:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-USB-to-Ethernet-Converter-using-LPC1837/m-p/556321#M15147</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2016-08-29T14:11:38Z</dc:date>
    </item>
  </channel>
</rss>