<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Secondary Bootloader LPC 54102</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Secondary-Bootloader-LPC-54102/m-p/555810#M15013</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by LorenSpencer on Tue Jan 19 23:50:16 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I has also solved the issue however luckily &lt;/SPAN&gt;&lt;A href="http://http://thetermpapers.net/college-term-papers/"&gt;best college term paper&lt;/A&gt;&lt;SPAN&gt; has helped me with that issue. They has built bootloader for&amp;nbsp; LPC54102 sensor and as well as sbl in order to control application. Both application has required the same changes.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:56:31 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:56:31Z</dc:date>
    <item>
      <title>Secondary Bootloader LPC 54102</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Secondary-Bootloader-LPC-54102/m-p/555808#M15011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by OldisGold on Wed Sep 30 11:44:46 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi NXP Support,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am working on building a secondary bootloader for the LPC54102 Sensor processing board. I am using LPCXpresso IDE v7.7.2. So far I built a SBL that can boot and pass control to the user application. I tried with two user applications blinky and sensorhub. Removed the board project from both so that the chip can be used on a custom board. Both applications work well independently without the SBL. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I load the sensor user applicaiton on top of the SBL it works as expected. However when I try to load the blinky it doesn't work. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I made the same changes on both the user applications. The cr_startup_lpc5410x.c has been modified as specified in AN11610 LPC5410x I2C SPI bootloader and also the flash start location have been modified. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please find attached image of SBL main.c code&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;OldisGold&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:56:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Secondary-Bootloader-LPC-54102/m-p/555808#M15011</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:56:30Z</dc:date>
    </item>
    <item>
      <title>Re: Secondary Bootloader LPC 54102</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Secondary-Bootloader-LPC-54102/m-p/555809#M15012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by OldisGold on Fri Oct 02 11:32:33 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Okay,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I solved the issue myself.&amp;nbsp; I just made sure that both applications had the same configurations. The sysinit.c file was probably looking for board.h. Once I removed all references for board.h same on both the blinky and sensorhub applications they worked just fine. &lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:56:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Secondary-Bootloader-LPC-54102/m-p/555809#M15012</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:56:31Z</dc:date>
    </item>
    <item>
      <title>Re: Secondary Bootloader LPC 54102</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Secondary-Bootloader-LPC-54102/m-p/555810#M15013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by LorenSpencer on Tue Jan 19 23:50:16 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I has also solved the issue however luckily &lt;/SPAN&gt;&lt;A href="http://http://thetermpapers.net/college-term-papers/"&gt;best college term paper&lt;/A&gt;&lt;SPAN&gt; has helped me with that issue. They has built bootloader for&amp;nbsp; LPC54102 sensor and as well as sbl in order to control application. Both application has required the same changes.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:56:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Secondary-Bootloader-LPC-54102/m-p/555810#M15013</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:56:31Z</dc:date>
    </item>
  </channel>
</rss>