<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC43xx default pins in output mode in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-default-pins-in-output-mode/m-p/555713#M14997</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by PhilYoung on Sun May 13 00:32:35 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;the pins should be outputs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;reset is a bit misleading since the boot loader always runs after reset, so don't assume that a pin takes its HW reset value, for many they will have the value set by&amp;nbsp; the boot loader which has to enable the memory interface to check for an image in external flash depending on the boot mode pins.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:38:58 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:38:58Z</dc:date>
    <item>
      <title>LPC43xx default pins in output mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-default-pins-in-output-mode/m-p/555712#M14996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by acristescu on Tue May 08 07:50:52 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am currently designing a board with LPC4330. I have observed that some of the pins have as function #0 (default function) output states. The pins are the followings (on my TQFP144 package):&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;- P4_7 -&amp;gt; LCD_DCLK&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- PF_4 -&amp;gt; SSP1_CLK&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- CLK0 -&amp;gt; EMC_CLK0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- CLK2 -&amp;gt; EMC_CLK3&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My questions are:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1) Are these really outputs after reset?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2) What are the waveforms or logic states after reset?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3) During reset they are Hiz or outputs?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for help.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:38:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-default-pins-in-output-mode/m-p/555712#M14996</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:38:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPC43xx default pins in output mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-default-pins-in-output-mode/m-p/555713#M14997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by PhilYoung on Sun May 13 00:32:35 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;the pins should be outputs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;reset is a bit misleading since the boot loader always runs after reset, so don't assume that a pin takes its HW reset value, for many they will have the value set by&amp;nbsp; the boot loader which has to enable the memory interface to check for an image in external flash depending on the boot mode pins.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:38:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-default-pins-in-output-mode/m-p/555713#M14997</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:38:58Z</dc:date>
    </item>
    <item>
      <title>Re: LPC43xx default pins in output mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-default-pins-in-output-mode/m-p/555714#M14998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by acristescu on Mon May 14 02:11:13 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks Phil for help.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using P4_7 and PF_4 in my schematic for some synchronization signals (IO) but I prefer them to be Hiz at boot (GPIO IN). My design will boot from SPIFI, will not use SSP1. Unfortunately I do not have a board in my hand to check these two pin signals with oscilloscope when LPC43xx boots from SPIFI. Is there any bootloader code published to take a look there?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:38:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-default-pins-in-output-mode/m-p/555714#M14998</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:38:59Z</dc:date>
    </item>
  </channel>
</rss>