<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Low cost CMSIS-DAP JTag a Kickstarter project in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Low-cost-CMSIS-DAP-JTag-a-Kickstarter-project/m-p/555424#M14951</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by yoko on Wed Jan 14 21:39:12 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;A href="http://https://www.kickstarter.com/projects/2112294877/idap-link-a-low-cost-full-features-debug-jtag"&gt;&lt;STRONG&gt;Project on Kickstarter&lt;/STRONG&gt;&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The IDAP-Link is a very low cost CMSIS-DAP JTAG debug probe with enhanced features. It can do more with it than just debugging. It will appears as a USB disk drive. This allows firmware flashing easily by copying the firmware file over without requiring any special flashing software and work instantly with any operating system. It provides a UART to USB bridge for communication between the target device and the PC. It also provides a regulated 3.3V to directly power the target device without addition power source by taking advantage of the USB power source. These feature turn the target device into mBed enable. It can be used as an ultra low cost solution to production programming. BSP is provide for use with Open Source CMSIS-DAP firmware from mBed.org which make it totally customizable.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]Support both SWD &amp;amp; JTAG mode Debug&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]compatibility with most IDE such as Keil, CrosWorks, Eclipse, etc..&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]Onboard 3.3V regulator to power the target device directly&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]UART to USB bridge for communication between target and PC&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]Turn target device into mBed enabled&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]Firmware flashing by drap &amp;amp; drop simply by copying file over&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]Supported on OS X, Linux, Wndows&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;Gang programming with IDAP-Link&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;With the drag &amp;amp; drop feature, it would be easy to do gang programming by connecting multiple IDAP-Link to a single PC via a USB hub. Each IDAP-Link then would appears to the PC as a USB drive. All that is left to do is to copy firmware file over to each drive. This could be accomplished by a batch command.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:54:19 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:54:19Z</dc:date>
    <item>
      <title>Low cost CMSIS-DAP JTag a Kickstarter project</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Low-cost-CMSIS-DAP-JTag-a-Kickstarter-project/m-p/555424#M14951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by yoko on Wed Jan 14 21:39:12 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;A href="http://https://www.kickstarter.com/projects/2112294877/idap-link-a-low-cost-full-features-debug-jtag"&gt;&lt;STRONG&gt;Project on Kickstarter&lt;/STRONG&gt;&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The IDAP-Link is a very low cost CMSIS-DAP JTAG debug probe with enhanced features. It can do more with it than just debugging. It will appears as a USB disk drive. This allows firmware flashing easily by copying the firmware file over without requiring any special flashing software and work instantly with any operating system. It provides a UART to USB bridge for communication between the target device and the PC. It also provides a regulated 3.3V to directly power the target device without addition power source by taking advantage of the USB power source. These feature turn the target device into mBed enable. It can be used as an ultra low cost solution to production programming. BSP is provide for use with Open Source CMSIS-DAP firmware from mBed.org which make it totally customizable.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]Support both SWD &amp;amp; JTAG mode Debug&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]compatibility with most IDE such as Keil, CrosWorks, Eclipse, etc..&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]Onboard 3.3V regulator to power the target device directly&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]UART to USB bridge for communication between target and PC&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]Turn target device into mBed enabled&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]Firmware flashing by drap &amp;amp; drop simply by copying file over&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]Supported on OS X, Linux, Wndows&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;Gang programming with IDAP-Link&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;With the drag &amp;amp; drop feature, it would be easy to do gang programming by connecting multiple IDAP-Link to a single PC via a USB hub. Each IDAP-Link then would appears to the PC as a USB drive. All that is left to do is to copy firmware file over to each drive. This could be accomplished by a batch command.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:54:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Low-cost-CMSIS-DAP-JTag-a-Kickstarter-project/m-p/555424#M14951</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:54:19Z</dc:date>
    </item>
    <item>
      <title>Re: Low cost CMSIS-DAP JTag a Kickstarter project</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Low-cost-CMSIS-DAP-JTag-a-Kickstarter-project/m-p/555425#M14952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by basicchip on Mon Sep 14 15:25:05 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I don't know if your kickstarter ever got off or not.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;We have published a design, schematic, BOM and gerbers for a low cost CMSIS-JTAG/SW board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/www.coridium.us/JTAG.html" target="test_blank"&gt;www.coridium.us/JTAG.html&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Too little margin in it for us to manufacture, and I expect clones or something similar will show up on eBay.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:54:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Low-cost-CMSIS-DAP-JTag-a-Kickstarter-project/m-p/555425#M14952</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:54:20Z</dc:date>
    </item>
  </channel>
</rss>