<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックSet input of SCT (State Configurable Timer) using a register instead of a pin</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Set-input-of-SCT-State-Configurable-Timer-using-a-register/m-p/555095#M14895</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wlamers on Fri Jun 28 07:33:33 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;From the manual it does not seem to be possible to set or clear the inputs of the State Configurable Timer using a register. It can only be done using physical pins it appears. I think it would be highly benificial to set the inputs in the application code by setting a register for example. The manual says that the SCT INPUT register in read-only (p838, table 665). Is there another way to set the inputs?&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;I tried using the SPGIO3 and SGPIO12 inputs, routing them using the GIMA to the SCT. While this works, it is still limited to 2 inputs. Another side note with this is that SGPIO3 seems bo be high on reset, which I find strange.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Bottom line: who knows a way to set the SCT inputs in code?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:40:46 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:40:46Z</dc:date>
    <item>
      <title>Set input of SCT (State Configurable Timer) using a register instead of a pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Set-input-of-SCT-State-Configurable-Timer-using-a-register/m-p/555095#M14895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wlamers on Fri Jun 28 07:33:33 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;From the manual it does not seem to be possible to set or clear the inputs of the State Configurable Timer using a register. It can only be done using physical pins it appears. I think it would be highly benificial to set the inputs in the application code by setting a register for example. The manual says that the SCT INPUT register in read-only (p838, table 665). Is there another way to set the inputs?&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;I tried using the SPGIO3 and SGPIO12 inputs, routing them using the GIMA to the SCT. While this works, it is still limited to 2 inputs. Another side note with this is that SGPIO3 seems bo be high on reset, which I find strange.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Bottom line: who knows a way to set the SCT inputs in code?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:40:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Set-input-of-SCT-State-Configurable-Timer-using-a-register/m-p/555095#M14895</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:40:46Z</dc:date>
    </item>
  </channel>
</rss>