<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Problem with LPC4330-Xplorer and LPC-Link(HID)</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-with-LPC4330-Xplorer-and-LPC-Link-HID/m-p/555077#M14891</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Willi.L on Fri Jun 28 05:59:45 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;I have a follow problem:&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;I use LPCExpresso (v5.2.4) and LPCXplorer4330.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;If I debug the LPC4330-Xplorer_LedToggle-Example (without changes) with LPC-Link2 (Debugger set to RedProbe), it works fine.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;If I debug the same axf.-file with LPC-Link (Debugger set to LPC-Link(HID)), it works not correct. I can debug, but the processor stays in systick_delay(),&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;because the SysTick_Handler(void) will not be run.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Have anyone idee, what is the cause?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:40:29 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:40:29Z</dc:date>
    <item>
      <title>Problem with LPC4330-Xplorer and LPC-Link(HID)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-with-LPC4330-Xplorer-and-LPC-Link-HID/m-p/555077#M14891</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Willi.L on Fri Jun 28 05:59:45 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;I have a follow problem:&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;I use LPCExpresso (v5.2.4) and LPCXplorer4330.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;If I debug the LPC4330-Xplorer_LedToggle-Example (without changes) with LPC-Link2 (Debugger set to RedProbe), it works fine.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;If I debug the same axf.-file with LPC-Link (Debugger set to LPC-Link(HID)), it works not correct. I can debug, but the processor stays in systick_delay(),&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;because the SysTick_Handler(void) will not be run.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Have anyone idee, what is the cause?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:40:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-with-LPC4330-Xplorer-and-LPC-Link-HID/m-p/555077#M14891</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:40:29Z</dc:date>
    </item>
  </channel>
</rss>