<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1778 iap entry 0x1FFF1FF0 data error</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-iap-entry-0x1FFF1FF0-data-error/m-p/554899#M14848</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;我创建了一个在ram中运行的代码准备测试iap功能。&lt;/P&gt;&lt;P&gt;1、如果我使用jlink工具先片擦除ROM。这是为了确保内部flash都是0xff。然后我在ram中进行仿真发现IAP的入口地址0x1FFF_1FF0处的数据都是0x0000_0000. 这时执行IAP进行flash操作就会出错。&lt;/P&gt;&lt;P&gt;2、如果我先下载一个比如闪灯的代码到flash 0地址开始处。在进行ram仿真，发现IAP的入口地址数据变成了0xbb1af7ff.这时就能使用iap进行flash操作。&lt;/P&gt;&lt;P&gt;请问是什么原因导致0x1fff1fff0 地址的数据出现错误&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Jun 2016 09:21:47 GMT</pubDate>
    <dc:creator>haopengtang</dc:creator>
    <dc:date>2016-06-21T09:21:47Z</dc:date>
    <item>
      <title>LPC1778 iap entry 0x1FFF1FF0 data error</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-iap-entry-0x1FFF1FF0-data-error/m-p/554899#M14848</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;我创建了一个在ram中运行的代码准备测试iap功能。&lt;/P&gt;&lt;P&gt;1、如果我使用jlink工具先片擦除ROM。这是为了确保内部flash都是0xff。然后我在ram中进行仿真发现IAP的入口地址0x1FFF_1FF0处的数据都是0x0000_0000. 这时执行IAP进行flash操作就会出错。&lt;/P&gt;&lt;P&gt;2、如果我先下载一个比如闪灯的代码到flash 0地址开始处。在进行ram仿真，发现IAP的入口地址数据变成了0xbb1af7ff.这时就能使用iap进行flash操作。&lt;/P&gt;&lt;P&gt;请问是什么原因导致0x1fff1fff0 地址的数据出现错误&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jun 2016 09:21:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-iap-entry-0x1FFF1FF0-data-error/m-p/554899#M14848</guid>
      <dc:creator>haopengtang</dc:creator>
      <dc:date>2016-06-21T09:21:47Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1778 iap entry 0x1FFF1FF0 data error</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-iap-entry-0x1FFF1FF0-data-error/m-p/554900#M14849</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;我手头没有LPC1778的板子，所以用LPC1788的板子做了个测试。&lt;/P&gt;&lt;P&gt;使用J-Link Commander工具完全擦除LPC1788芯片后，读取0x1FFF1FF0地址的值如下：&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41788i27682849EF8637FA/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;如果你手头也有J-Link工具，也可以测试一下（输入下列命令）：&lt;/P&gt;&lt;P&gt;usb&lt;/P&gt;&lt;P&gt;device ？ （选择NXP LPC1778）&lt;/P&gt;&lt;P&gt;erase all&lt;/P&gt;&lt;P&gt;mem32 0x1fff1ff0 0x10&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Segger J-Link Commander 软件可以从&lt;A href="https://www.segger.com/downloads/jlink"&gt;这里&lt;/A&gt;下载。&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 02:08:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-iap-entry-0x1FFF1FF0-data-error/m-p/554900#M14849</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-07-28T02:08:21Z</dc:date>
    </item>
  </channel>
</rss>