<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Reading more than 64 bytes and using a Circular buffer suing USBD API on lpc43xx in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Reading-more-than-64-bytes-and-using-a-Circular-buffer-suing/m-p/553496#M14573</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by pra18 on Wed Nov 12 09:31:46 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am migrating from UART to a USB CDC on my custom board. The UART on my custom board is handling 256 byte receptions currently and also on USB CDC will this required to be supported.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The Bulk endpoint maximum is 64 bytes in which case, for 256 byte transfers there needs to be some mechanism to handle mostly a circle buffer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I see that in&amp;nbsp; the USB VCOM example of lpcopen 2_0_12 , and in&amp;nbsp; Bulk EVT_OUT handler code , the ReadEP is called and this is where the functionality needs to be added to support more than 64 bytes&amp;nbsp; and also there is needed a helper function like Read to assist this Build EVT_OUT.I see something like VCOMBRead in that example.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any suggestions how this can be achieved and any examples using a circular buffer that can be referred to in this case?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks, &lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:37:04 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:37:04Z</dc:date>
    <item>
      <title>Reading more than 64 bytes and using a Circular buffer suing USBD API on lpc43xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Reading-more-than-64-bytes-and-using-a-Circular-buffer-suing/m-p/553496#M14573</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by pra18 on Wed Nov 12 09:31:46 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am migrating from UART to a USB CDC on my custom board. The UART on my custom board is handling 256 byte receptions currently and also on USB CDC will this required to be supported.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The Bulk endpoint maximum is 64 bytes in which case, for 256 byte transfers there needs to be some mechanism to handle mostly a circle buffer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I see that in&amp;nbsp; the USB VCOM example of lpcopen 2_0_12 , and in&amp;nbsp; Bulk EVT_OUT handler code , the ReadEP is called and this is where the functionality needs to be added to support more than 64 bytes&amp;nbsp; and also there is needed a helper function like Read to assist this Build EVT_OUT.I see something like VCOMBRead in that example.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any suggestions how this can be achieved and any examples using a circular buffer that can be referred to in this case?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks, &lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:37:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Reading-more-than-64-bytes-and-using-a-Circular-buffer-suing/m-p/553496#M14573</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:37:04Z</dc:date>
    </item>
  </channel>
</rss>