<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Interrupt from concurrent CAN channels stopping in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Interrupt-from-concurrent-CAN-channels-stopping/m-p/553357#M14541</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Randy Nuss on Sat Mar 16 14:14:07 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using both CAN channels of the lpc4337.&amp;nbsp; Each physical CAN bus is a 250kHz bus -what the actual data rates are I can't say for sure.&amp;nbsp; A single channel is processed fine.&amp;nbsp; When both channels are enabled, I receive data for a short time (few seconds maybe) then CAN-receive interrupts just stop.&amp;nbsp; This never occurred when I interfaced to the very same buses using an lpc17xx.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the event-router interrupt for the CCAN which provides a single interrupt for either CAN channel.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could there be an arbitration issue with the two interrupt sources and the single event-router interrupt?&amp;nbsp; I noticed there are separate interrupts available for the two CAN channels -maybe I should try those instead of the event-router?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is a halt of interrupts possible if data isn't read in time?&amp;nbsp; Is it possible this is not a concurrent channel issue but a higher data issue?&amp;nbsp; I am running the lpc4337 at 90MHz, but again the lpc17xx was running slower and doing ok.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I haven't been back on the hardware yet to try and trap any error conditions the CAN interrupt handler might indicate.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:38:10 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:38:10Z</dc:date>
    <item>
      <title>Interrupt from concurrent CAN channels stopping</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Interrupt-from-concurrent-CAN-channels-stopping/m-p/553357#M14541</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Randy Nuss on Sat Mar 16 14:14:07 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using both CAN channels of the lpc4337.&amp;nbsp; Each physical CAN bus is a 250kHz bus -what the actual data rates are I can't say for sure.&amp;nbsp; A single channel is processed fine.&amp;nbsp; When both channels are enabled, I receive data for a short time (few seconds maybe) then CAN-receive interrupts just stop.&amp;nbsp; This never occurred when I interfaced to the very same buses using an lpc17xx.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the event-router interrupt for the CCAN which provides a single interrupt for either CAN channel.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could there be an arbitration issue with the two interrupt sources and the single event-router interrupt?&amp;nbsp; I noticed there are separate interrupts available for the two CAN channels -maybe I should try those instead of the event-router?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is a halt of interrupts possible if data isn't read in time?&amp;nbsp; Is it possible this is not a concurrent channel issue but a higher data issue?&amp;nbsp; I am running the lpc4337 at 90MHz, but again the lpc17xx was running slower and doing ok.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I haven't been back on the hardware yet to try and trap any error conditions the CAN interrupt handler might indicate.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:38:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Interrupt-from-concurrent-CAN-channels-stopping/m-p/553357#M14541</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:38:10Z</dc:date>
    </item>
  </channel>
</rss>