<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC4330 ethernet- remote wake up frame filter.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4330-ethernet-remote-wake-up-frame-filter/m-p/553268#M14531</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Krishnakumar on Mon Sep 29 04:38:21 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi folks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In LPC4330 ethernet, It has a register called remote wake up frame filter(WAKEUPFMFILTER_REG) which is used for wake on lan configuration by wake up farme.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The WAKEUPFMFILTER has a field called "filter i CRC_16" which is 16 bits wide. In the document UM10503.pdf it's given that this "filter i crc_16" field contains CRC_16 value calculated for the pattern and the byte mask programmed to the wake-up filter register block.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But the byte mask is of 32 bits and how a field of 16 bits wide that is "filter i CRC_16" contains 16 bits CRC(CRC_16 for pattern) and the 32 bits byte mask. Let me know, if is there any logic behind that?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks and regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Krishnakumar Kulkarni&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:37:42 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:37:42Z</dc:date>
    <item>
      <title>LPC4330 ethernet- remote wake up frame filter.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4330-ethernet-remote-wake-up-frame-filter/m-p/553268#M14531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Krishnakumar on Mon Sep 29 04:38:21 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi folks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In LPC4330 ethernet, It has a register called remote wake up frame filter(WAKEUPFMFILTER_REG) which is used for wake on lan configuration by wake up farme.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The WAKEUPFMFILTER has a field called "filter i CRC_16" which is 16 bits wide. In the document UM10503.pdf it's given that this "filter i crc_16" field contains CRC_16 value calculated for the pattern and the byte mask programmed to the wake-up filter register block.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But the byte mask is of 32 bits and how a field of 16 bits wide that is "filter i CRC_16" contains 16 bits CRC(CRC_16 for pattern) and the 32 bits byte mask. Let me know, if is there any logic behind that?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks and regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Krishnakumar Kulkarni&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:37:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4330-ethernet-remote-wake-up-frame-filter/m-p/553268#M14531</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:37:42Z</dc:date>
    </item>
  </channel>
</rss>