<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC43xx SDRAM working at high frequencies</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-SDRAM-working-at-high-frequencies/m-p/553150#M14523</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mc on Tue Jun 30 07:11:51 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;150MHz SDRAM frequency is out of specification.The maximum speed is 120MHz. In this case your Core clock should also run at 120MHz.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:37:32 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:37:32Z</dc:date>
    <item>
      <title>LPC43xx SDRAM working at high frequencies</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-SDRAM-working-at-high-frequencies/m-p/553149#M14522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by michele_sponchiado_windows on Tue Jun 30 05:59:20 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the LPC43xx and I've evaluated some boards (WaveShare 4357, EA4357).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In none of these I was able to achieve a SDRAM working frequency bigger than 150MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If I increase the frequency to the next PLL step, I never found a setup where the system works fine, because typically HardFault arise when e.g. using the external memory as a memory pool, or as a heap etc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried changing sfsclk settings as set in AN11508, changing the emc delay clock, using only the CLK1 signal to interface the SDRAM, but without success.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has anyone every succeded running a SDRAM to frequencies higher than 150MHz?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:37:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-SDRAM-working-at-high-frequencies/m-p/553149#M14522</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:37:31Z</dc:date>
    </item>
    <item>
      <title>Re: LPC43xx SDRAM working at high frequencies</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-SDRAM-working-at-high-frequencies/m-p/553150#M14523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mc on Tue Jun 30 07:11:51 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;150MHz SDRAM frequency is out of specification.The maximum speed is 120MHz. In this case your Core clock should also run at 120MHz.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:37:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-SDRAM-working-at-high-frequencies/m-p/553150#M14523</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:37:32Z</dc:date>
    </item>
  </channel>
</rss>