<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC5411x MCU family announced</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5411x-MCU-family-announced/m-p/553094#M14514</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Tue Feb 23 01:45:04 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP Semiconductors N.V. (NASDAQ: NXPI) today introduced its next-generation family of low-power, multi-market MCUs – the LPC5411x. With today’s introduction, NXP extends its LPC54000 series of MCUs with improved power efficiency, a host of serial peripherals, flexible run-modes, autonomous operations when the CPU is not active and voice-detection DSP hardware.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPC5411x are ARM Cortex-M4 based microcontrollers for embedded applications.These devices include an ARM Cortex-M0+ coprocessor, up to 192 KB of on-chip SRAM, up to 256 KB on-chip flash, full-speed USB device interface with Crystal-less operation, a DMIC subsystem with PDM microphone interface and I²S, five general-purpose timers, one SCTimer/PWM, one RTC/alarm timer, one 24-bit Multi-Rate Timer (MRT), a Windowed Watchdog Timer (WWDT), eight flexible serial communication peripherals (each of which can be a USART, SPI, or I²C interface), and one 12-bit 5.0 Msamples/sec ADC, and a temperature sensor&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For more information see:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]&lt;/SPAN&gt;&lt;A href="http://http://media.nxp.com/phoenix.zhtml?c=254228&amp;amp;p=irol-newsArticle&amp;amp;ID=2141974"&gt;LPC5411x Press release&lt;/A&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]&lt;/SPAN&gt;&lt;A href="http://http://www.nxp.com/pages/:LPC5411X"&gt;LPC5411x Product page&lt;/A&gt;&lt;BR /&gt;&lt;SPAN&gt;[/list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:53:44 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:53:44Z</dc:date>
    <item>
      <title>LPC5411x MCU family announced</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5411x-MCU-family-announced/m-p/553094#M14514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Tue Feb 23 01:45:04 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP Semiconductors N.V. (NASDAQ: NXPI) today introduced its next-generation family of low-power, multi-market MCUs – the LPC5411x. With today’s introduction, NXP extends its LPC54000 series of MCUs with improved power efficiency, a host of serial peripherals, flexible run-modes, autonomous operations when the CPU is not active and voice-detection DSP hardware.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPC5411x are ARM Cortex-M4 based microcontrollers for embedded applications.These devices include an ARM Cortex-M0+ coprocessor, up to 192 KB of on-chip SRAM, up to 256 KB on-chip flash, full-speed USB device interface with Crystal-less operation, a DMIC subsystem with PDM microphone interface and I²S, five general-purpose timers, one SCTimer/PWM, one RTC/alarm timer, one 24-bit Multi-Rate Timer (MRT), a Windowed Watchdog Timer (WWDT), eight flexible serial communication peripherals (each of which can be a USART, SPI, or I²C interface), and one 12-bit 5.0 Msamples/sec ADC, and a temperature sensor&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For more information see:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]&lt;/SPAN&gt;&lt;A href="http://http://media.nxp.com/phoenix.zhtml?c=254228&amp;amp;p=irol-newsArticle&amp;amp;ID=2141974"&gt;LPC5411x Press release&lt;/A&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]&lt;/SPAN&gt;&lt;A href="http://http://www.nxp.com/pages/:LPC5411X"&gt;LPC5411x Product page&lt;/A&gt;&lt;BR /&gt;&lt;SPAN&gt;[/list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:53:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5411x-MCU-family-announced/m-p/553094#M14514</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:53:44Z</dc:date>
    </item>
  </channel>
</rss>