<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 433x M4 USB stops to work(cannot enumeration ) when enable sgpio/DMA in M0 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/433x-M4-USB-stops-to-work-cannot-enumeration-when-enable-sgpio/m-p/552996#M14497</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jpplus on Mon Dec 08 02:51:29 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I meet a problem that when I enable sgpio/DMA in M0,&amp;nbsp; then in M4 the USB cannot enumueration and stop working.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;if I don't use SGPIO, then USB works perferct. The USB is configured as CDC/ACM VCOM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the SGPIO is used like I2S to triigger DMA as audio application. The SGPIO is confgured and run in M0. In M4, the USB is init and run. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Enabling individual SGPIO in M0 or&amp;nbsp; enabling USB in M4 is Ok, but it seems they cannot run together.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;As USB and SGPIO audio application can run, the pin mux and clock should set correctly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;my steps are:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1) init M4, init all clock&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2) start M0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3) start M4 USB&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4) start M0 codec, DMA, sgpio&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;if I skip the M0 DMA init or sgpio init, then the M4 USB can work. If I init DMA and enable SGPIO( I think DMA interrupt will come then), then USB stop to work.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;or I don't plug in USB cable, then it is still working, and my audio app can work. But after I plug in the cable, the audio stop working and USB cannot ENU.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;any idea about that? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;any possible of conflict on these two(sgpio/DMA, USB)?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;please help, as I indeed need the USB to stream or configure some data.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 18:38:45 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T18:38:45Z</dc:date>
    <item>
      <title>433x M4 USB stops to work(cannot enumeration ) when enable sgpio/DMA in M0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/433x-M4-USB-stops-to-work-cannot-enumeration-when-enable-sgpio/m-p/552996#M14497</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jpplus on Mon Dec 08 02:51:29 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I meet a problem that when I enable sgpio/DMA in M0,&amp;nbsp; then in M4 the USB cannot enumueration and stop working.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;if I don't use SGPIO, then USB works perferct. The USB is configured as CDC/ACM VCOM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the SGPIO is used like I2S to triigger DMA as audio application. The SGPIO is confgured and run in M0. In M4, the USB is init and run. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Enabling individual SGPIO in M0 or&amp;nbsp; enabling USB in M4 is Ok, but it seems they cannot run together.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;As USB and SGPIO audio application can run, the pin mux and clock should set correctly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;my steps are:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1) init M4, init all clock&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2) start M0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3) start M4 USB&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4) start M0 codec, DMA, sgpio&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;if I skip the M0 DMA init or sgpio init, then the M4 USB can work. If I init DMA and enable SGPIO( I think DMA interrupt will come then), then USB stop to work.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;or I don't plug in USB cable, then it is still working, and my audio app can work. But after I plug in the cable, the audio stop working and USB cannot ENU.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;any idea about that? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;any possible of conflict on these two(sgpio/DMA, USB)?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;please help, as I indeed need the USB to stream or configure some data.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:38:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/433x-M4-USB-stops-to-work-cannot-enumeration-when-enable-sgpio/m-p/552996#M14497</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:38:45Z</dc:date>
    </item>
    <item>
      <title>Re: 433x M4 USB stops to work(cannot enumeration ) when enable sgpio/DMA in M0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/433x-M4-USB-stops-to-work-cannot-enumeration-when-enable-sgpio/m-p/552997#M14498</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jpplus on Tue Dec 09 01:59:39 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;any clues/hints are really appeciated.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:38:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/433x-M4-USB-stops-to-work-cannot-enumeration-when-enable-sgpio/m-p/552997#M14498</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:38:46Z</dc:date>
    </item>
  </channel>
</rss>