<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC4370 HSADC with DMA</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-HSADC-with-DMA/m-p/552919#M14481</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been looking for example codes for HSADC using DMA on LPC-Link2 board. All sources I could find seems to point to the Labtool code. There is no example code using the current lpcopen 2.12 library.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question:&lt;/P&gt;&lt;P&gt;Is there an example code using lpcopen 2.12? If yes, can you kindly point out the source? If not, any reasons that it does not exist? (For example, maybe lpcopen 2.12 is not able to support the feature?)&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Jul 2016 21:37:34 GMT</pubDate>
    <dc:creator>mtenw</dc:creator>
    <dc:date>2016-07-29T21:37:34Z</dc:date>
    <item>
      <title>LPC4370 HSADC with DMA</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-HSADC-with-DMA/m-p/552919#M14481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been looking for example codes for HSADC using DMA on LPC-Link2 board. All sources I could find seems to point to the Labtool code. There is no example code using the current lpcopen 2.12 library.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question:&lt;/P&gt;&lt;P&gt;Is there an example code using lpcopen 2.12? If yes, can you kindly point out the source? If not, any reasons that it does not exist? (For example, maybe lpcopen 2.12 is not able to support the feature?)&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jul 2016 21:37:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-HSADC-with-DMA/m-p/552919#M14481</guid>
      <dc:creator>mtenw</dc:creator>
      <dc:date>2016-07-29T21:37:34Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4370 HSADC with DMA</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-HSADC-with-DMA/m-p/552920#M14482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi mtenw,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The resources we have on HSADC are LPCOpen examples and the Labtool solution for now, but I think the following thread might be helpful for you:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/429528"&gt;How to achieve 80MHz using DMA from LPC4370's HSADC?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Carlos Mendoza&lt;/P&gt;&lt;P&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Aug 2016 23:04:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-HSADC-with-DMA/m-p/552920#M14482</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2016-08-15T23:04:40Z</dc:date>
    </item>
  </channel>
</rss>